STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32f439 supported compiler tool

Posted on March 14, 2014 at 07:03hi all as iam going to work on STM32F439 controller ,i come to know coocox tool is not supporting stm32f439 controller ,can any one let me know that what is the  supported compiler to proceed me further..thanks in ad...

STM32F417 ADC DMA synchronization

Posted on April 24, 2014 at 17:31Hi All, i'm running ADC example from STM's examples, and i'm having repeated values on 100kHz sinusoidal signal , probably it's not possible to sample it to have good resolution but it's only test for repeating , if ...

STM32F4 compiler

Posted on April 22, 2014 at 22:23Hi all, does anybody have running gcc with simd for Cortex-M4 ? Kind regards,

TIM_6Steps

Posted on April 23, 2014 at 16:54Hi all together, I want to test the TIM_6Steps from the ''STM32F4xx_DSP_StdPeriph_Lib_V1.3.0'' Library with the STM32F4-Discovery-Board which uses the STM32F407VGT6. The compiler does not send any error but I do not ...

Missing TIM4 definition??

Posted on April 22, 2014 at 22:05 Hello All, I trying the following configuration of TIM4 on STM32L152 void Timer4Init(void) { RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM4, ENABLE); // Zero cross in - counter start CH3 ...

Tom by Associate II
  • 2180 Views
  • 3 replies
  • 0 kudos

STM32CUBE and USB framework

Posted on April 23, 2014 at 15:46Has the USB framework supplied with STM32CubeF4 been completely rewritten or is it  the USB-Host-Device_Lib_V2.1.0?

thierry1 by Associate II
  • 1138 Views
  • 2 replies
  • 0 kudos

Bug HAL_NVIC_EnableIRQ(EXTI9_5_IRQn)

Posted on April 14, 2014 at 17:04Don't know if this is an oversight or normal. When I configure a pin with CubeMX to be ''External Interrupt Mode with Falling edge trigger detection'' for example, and enable the interrupt in the NVIC configuration, ...

joe by Associate III
  • 1147 Views
  • 1 replies
  • 0 kudos

SPI data transfer using DMA with a L6470 dSPIN device

Posted on April 22, 2014 at 14:24Hey everyone, I am using a STM32F0-Discovery with a L6470 stepper driver IC attached. As a sofwtare basis I currently use ChibiOS. I am able to command the L6470 utilizing the DMA controller for SPI data transfer but...

Chip Select Pin in SPI with STM32F4Discovery

Posted on April 23, 2014 at 23:20Hi everyone, I'm trying to implement SPI on stm32f4discovery kit here's the code I found on some blog<b>#include ''stm32f4_discovery.h''#include <stm32f4xx.h>#include <stm32f4xx_spi.h>void delay(uint32_t cnt);// this...