Skip to main content
tzewan
Associate
September 13, 2013
Question

No NAND flash on STM3220G-Eval

  • September 13, 2013
  • 2 replies
  • 787 views
Posted on September 13, 2013 at 12:20

Hi all,

I would like to evaluate the NAND flash interface with the STM3220G-Eval board. However, this board is not populated with the NAND flash, although the board has an estate-area for it. If I were to buy a flash, I do not have the tools to solder the BGA-type flash onto it either. Are there any ways where I can evaluate flash functionality on STM32 F2 series? I am using IAR as the compiler. I do have another STM3210E-Eval which has a populated flash. However, this board is based on F2 series, which is not what our team wants in the final design.

I would appreciate any feedback or ideas. Thanks in advance.

#nand-stm32f2-flash
This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
September 13, 2013
Posted on September 13, 2013 at 12:57

Go to eBay (or eCommerce site of choice), and dig around

http://www.ebay.com/itm/STM32F207ZG-module-HY-STM32F2xxCore144-Core-Dev-Board-/170874320152?pt=LH_DefaultDomain_0&hash=item27c8e73518

Alternatively if your team can solder/desolder QFP's get a F4 board and swap out the processor.
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
tzewan
tzewanAuthor
Associate
September 20, 2013
Posted on September 20, 2013 at 17:40

Thank you for your advice..