Skip to main content
m_fawaz
Associate
September 20, 2013
Question

STM32F4 Discovery: Write data to a memory key using the micro USB

  • September 20, 2013
  • 1 reply
  • 665 views
Posted on September 20, 2013 at 20:59

Dear Sirs,

Knowing that I want to log the data that the controller of the STM32F4 discovery is reading from the sensors, I need to write the data in a .csv format on a memory key using the micro USB.

Do you have a link to an example/tutorial that can help me in accomplishing the above? If not can you please provide me with the guidelines?

It is worthy of a note that I am new to the STM32F4 discovery and that I already accomplished some simple proof of concept using the CoIDE of CooCox.

Awaiting your help,

Best regards,

Marc

#stm32f4-discovery:-micro-usb
This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
September 20, 2013
Posted on September 20, 2013 at 21:18

http://www.st.com/st-web-ui/static/active/en/resource/technical/document/application_note/DM00039672.pdf

STM32F4-Discovery_FW_V1.1.0\Project\FW_upgrade

Key take away : FatFs access to USB attached Flash or IDE drive

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..