STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Scary java crash in CubeMX

Posted on April 23, 2014 at 14:39When you enable any part in the ADC (F401RET 64pin mcu) you get a java-crash:Apr 23, 2014 2:03:11 PM com.st.microxplorer.util.LogicalParser checkConditionSEVERE: nullcom.bestcode.mathparser.ParserException: ExpNtVld ...

belhage by Associate
  • 993 Views
  • 2 replies
  • 0 kudos

independent DAC Channel triggers on STMF3XX

Posted on April 21, 2014 at 07:55Hi,I am using STM32F303 to generate 2 sine-waves  on DAC_Channel1 and DAC_Channel2.I use one lookup table to generate the sine-wave. And I succeded to generate sine-waves on both channels, but the generated signals h...

bugra by Associate II
  • 1454 Views
  • 2 replies
  • 0 kudos

STM32F429I-Disco SDRAM disable question

Posted on April 27, 2014 at 02:22 .ExternalClassFB32C94191F74142971920E4B5386622 P {margin-bottom:0.08in;} I have the STM32F429I Disco board and would like to use more GPIOs than the 27 free ones available in the current board configuration.I see...

gbarbour by Associate III
  • 1423 Views
  • 3 replies
  • 0 kudos

stm32f4 pwm input example

Posted on April 26, 2014 at 20:44Is anybody willing to explain ''The TIMxCLK frequency is set to SystemCoreClock/4 (Hz). The Prescaler is 0, so the counter clock is SystemCoreClock/2 (Hz). '' Is TIMxCLK not the same as counter clock? Thanks, Jonath...

jono-tree by Associate II
  • 1685 Views
  • 4 replies
  • 0 kudos

STM32 and computational demands

Posted on April 25, 2014 at 17:13Hello everyoneI had this question in the back of my mind for some time now, i have a vague answer, but that is not what engineers are about -precision , right !?  :)The question pertains to any MCU or DSP, how do you...

STM32CubeMX V1.1.0 + SDRAM

Posted on April 25, 2014 at 03:35Greetings all,I'm trying to use STM32CubeMX to build a configuration for the EMCraft STM32F4 SOM. In trying to get the SDRAM functional and I believe I have the settings correct; however it looks like the generated c...

malcolm23 by Associate III
  • 1664 Views
  • 5 replies
  • 0 kudos

Can not use MCO output in VirtualComport_Loopback project

Posted on April 25, 2014 at 15:16Hi, all,    I use STM32F103VCT6 and VirtualComport_Loopback project for usb communication, the usb part works fine.     Now, I try to output the MCO at PA8, failed.void MCO_Config(void){ GPIO_InitTypeDef is;  RCC_APB...

chenbo by Associate
  • 1205 Views
  • 2 replies
  • 0 kudos

STM32F3 USART1 RX DMA

Posted on April 24, 2014 at 15:59 Hi all, Hoping to get a second pair of eyes on this code. I'm trying to capture large amounts of data from USART1 using DMA on an F30x series MCU. So far no luck - feels like I'm looking past an ob...

connect by Associate II
  • 2870 Views
  • 5 replies
  • 0 kudos

Confusion with DMA

Posted on April 25, 2014 at 22:00I am using an STM32F050G6 processor and using DMA to read 4 AD channels.  I am a little confused on how to control the order of the DMA reads of the ADC.Currently my code is set up to read channels 6,7,8,9 (PA6,7 PB0...

ebommer by Associate II
  • 1063 Views
  • 2 replies
  • 0 kudos

how to collect 50000 data points samples.

Posted on April 22, 2014 at 00:13I have to store 50000 samples. The information would be stored in an Array. Unfortunately the maximum size my program allows me to allocate the array space is 10000 because it complains could not allocate block. how ...