STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ST-LINK/V2 and Win7 64-bit

Posted on August 21, 2012 at 22:28Has anyone tried using the ST-LINK CLI.exe in windows 64-bit? Is there a way to make win7 run it as 32-bit?

pyoung by Associate
  • 4463 Views
  • 10 replies
  • 0 kudos

software camera interface

Posted on May 06, 2014 at 12:38 Hi all, I'm working on the example using the Omnivision camera ov2640, but I'm not sure about the resolution of the image coming from the camera. I would like to configure the camera with QQVGA resoluti...

ines by Associate II
  • 2866 Views
  • 4 replies
  • 0 kudos

FATFS Directory Size

Posted on May 07, 2014 at 15:08Does anyone know if there's a command to get the size of a directory in Chan's FATFS or will I need to go the directory and just tally up all the file sizes?

Delay between SPI bytes

Posted on May 07, 2014 at 15:53Using STM3220G-EVAL with my serial FLASH added to board. I am writing to a serial flash via the SPI port. My clock speed is 30Mhz. All is working fine, but I was expecting less delay between the SPI clock transfers. My...

gary2 by Associate
  • 1789 Views
  • 2 replies
  • 0 kudos

is there any external tool that could access EEPROM?

Posted on May 05, 2014 at 04:37Hi all,I'm using stm32l152rtc6 with built-in eeprom (8k).  I wonder if there's any tool at the host side that allows me to read/write the eeprom other than using ST library code for the mcu? (STM32L1xx_StdPeriph_Lib_V1...

STM32 clock Jitter on TIM4

Posted on April 02, 2014 at 08:56Hello everyone, I'm using STM32F100V8 and I configured TIM4 to generate a square wave (for uart sw). The TIM4 is so configured and should have the highest priority:   TIM_TimeBaseStructInit(&TIM_TimeBaseStructure);  ...

fernando by Associate II
  • 5856 Views
  • 8 replies
  • 0 kudos

STM32F407VG

Posted on May 05, 2014 at 12:44HI,It is possible to use the graphical library from ST to create a graphical application with STM32F407?  What about the LCD ?Best Regards ,

amal18 by Associate II
  • 1514 Views
  • 4 replies
  • 0 kudos

generating a PWM reference signal(Modem)

Posted on May 02, 2014 at 21:34Hello everyone,      I have a PWM signal generated from an external source and I want to create a reference signal from this one. First this signal is of constant duty cycle (I want to create a reference signal here), ...

I2C Slave Example

Posted on April 27, 2014 at 19:56Hi I'm working on STM32F401 disco EVB with the Standard Peripherals Library,Where i can find a working example on I2C slave?  

gil23 by Associate III
  • 3965 Views
  • 12 replies
  • 0 kudos