User Activity

Posted on April 14, 2014 at 10:56Hello everybody , I have a firmware which runs whose offset adress is 0x9000 and on stm32f105RC (256 KB Flash, 64K Ram). It is a iap sw that runs on stm32f205 I am trying it to run on stm32f105.NVIC_SetVectorTable(NV...
Posted on January 28, 2014 at 15:02Hello, USB Virtual Com Port example doesn't work on device modeI have a uC card wtih stm32f107 which works host and  FS mode, reads Flash disc.. Now I am trying eval vcp example, I made necessary changes but it doe...
Posted on January 28, 2014 at 15:01Hello, I have a uC card wtih stm32f107 which works host and  FS mode, reads Flash disc.. Now I am trying eval vcp example, I made necessary changes but it doesnt work even I put break points on main and systick. So...
Posted on December 20, 2013 at 16:40Hi,I work for an electronics company and we basically code stm32 F1 & F2 microcontrollers. Actually, my question is that how I can simulate the entire circuit  using a program like Proteus. However, as far as I kn...
Posted on December 03, 2013 at 14:48Hello I want to use 2 usb otg peripheral units of stm32f205 MCU to transfer .wav files one to other.. Where can I find source codes from? Do you have any idea or suggestion? What problems do you think I have by us...
Kudos from