STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F429 HardFault

Posted on June 22, 2014 at 17:47Hi everybodyI am trying to get a control system with a PD controller and a Kalman filter up and running on my STM32F429 discovery board.The Kalman filter receives data gathered by two sensors and calculates an estimat...

ben by Associate II
  • 1040 Views
  • 1 replies
  • 0 kudos

STM32F1 ADC+DMA problem

Posted on June 22, 2014 at 03:09 Hi! I would like to ask you for some help- I wrote a code to get ADC values from 8 channels (regular group). After each conversion there has to be of course DMA request. I wrote everything and... all I ge...

maciek by Associate II
  • 1760 Views
  • 4 replies
  • 0 kudos

SPI master with DMA - problem

Posted on June 19, 2014 at 15:29Hello,I'm trying to use SPI master with DMA in full duplex to communicate with accelerometer. I don't want to use DMA interrupts (or should I?).I've managed to activate the SPI with polling mode and got the correct re...

zoharr by Associate II
  • 4558 Views
  • 9 replies
  • 0 kudos

New STM32L0 ultra-low-power (Cortex-M0+)

Posted on February 11, 2014 at 18:02STMicroelectronics has announced the New STM32 Ultra-low-power MCU ARM CortexTM-M0+ based: STM32L0 SeriesThe new STM32L0 ultra-low-power  series features a 12-bit Analog-to-Digital Converter (ADC) that sets a new ...

STM32L0 & Nucleo availability?

Posted on May 08, 2014 at 18:21Has anyone heard concrete information about availability of the new STM32L0 series MCUs and the associated Nucleo dev kit?I'm very eager to get started on a design using these new devices, but despite an April 30 press...

kris by Associate
  • 1424 Views
  • 3 replies
  • 0 kudos

Want to change to TIM9_CH1 point to PE5 in STM32Cube_FW_F4_V1.1.0\Projects\STM324x9I_EVAL\Examples\TIM\TIM_PWMOutput

Posted on June 19, 2014 at 04:54I want to change to TIM9_CH1 point to PE5 in STM32Cube_FW_F4_V1.1.0\Projects\STM324x9I_EVAL\Examples\TIM\TIM_PWMOutput. The main.h is: ~~~~~~~~~~ #define TIMx                           TIM3 #define TIMx_CLK_ENABLE    ...

Linda by Associate II
  • 1953 Views
  • 4 replies
  • 0 kudos

I2C2 busy - SDA being pulled low without any slave attached

Posted on June 20, 2014 at 08:54 I'm trying to configure the I2C2 on an STM32F401 chip. The I2C1 is working fine, but the I2C2 is always returning HAL_BUSY. After initializing the GPIO port the SDA line is being pulled low, but no slave device i...

Jacob L by Associate II
  • 2368 Views
  • 3 replies
  • 0 kudos

STM32CubeMX Changes my Debug Port to JTAG

Posted on May 28, 2014 at 20:20I am using the STM32F4 Discovery board with the Debug Port set to SW for the ST-Link debugger. Development is in stages, so I run STM32CubeMX to set a peripheral, debug the resulting code, then pull in another peripher...