Question
stm32f4 usart max speed
Posted on April 02, 2014 at 11:26
I'm using stm32f407 combined with ftdi232h usb-serial converter.
Every byte I call an interrupt and send back the same byte to check. This works fine with baud rate to 115200. I have tried to force best baud rate (theoretically I can force to 9Mbaud). I have tried 1Mbaud, 3Mbaud and others but the interrupt read correctly only first byte, second is totally corrupt (for example I send value 3 and read 191). Does someone have experience how much I can force baud rate with a similar system? If I use DMA I improve the situation? How much? Is there some working example with high baud rate? Thanks. #stm32f4 #rs232 #usart