STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

CAN message

Posted on August 21, 2014 at 20:08Hi, I am trying to use CANbus on STM32F303VC6. I get it working in loopback mode. But the message is not getting sent in Normal mode. I have turned on SB21 and SB22 to connect the ports PA11 and PA12 to P2. When I d...

rizwin by Associate II
  • 1407 Views
  • 3 replies
  • 0 kudos

Sharing PA5 between HS USB and DAC2 on STM32F4

Posted on August 16, 2014 at 06:06HiI have problem in sharing the PA5 functionality on STM32f407IGT6.As I need to use both of DACs in my design, and HS_ULPI_CK is also routed only on that pin (there is no multiplex to any other pins).I can not use O...

sbsohrabi by Associate II
  • 2197 Views
  • 5 replies
  • 0 kudos

STM32F429 Discovery SPI Registers

Posted on August 21, 2014 at 16:14 I am trying to use theSTM32F429 Discovery boardin order to communicate in a transmit only mode to an LCD over SPI. However, every time I write to the data register to output, I see nothing get loaded in my debug...

cns1307 by Associate II
  • 1371 Views
  • 6 replies
  • 0 kudos

Can TIM16 & TIM17 be used in external clock source mode1?

Posted on September 04, 2013 at 18:42Hi, I would like to know if TIM16 and TIM17 can be used in external clock source mode 1. There is any reference in the Reference Manual that it doesn't. So I suppose it is possible. I develop my board and now I w...

tecnico23 by Associate II
  • 1035 Views
  • 1 replies
  • 0 kudos

Encoder mode - Prescaler or external trigger filter

Posted on August 21, 2014 at 14:46Hi everyone, I've been working on the STM32F4 and I would like to count pulses from some odometer. There are two types of odometer, the ones that output two signal in quadrature and the other that output pulse on ...

maxime2 by Associate
  • 1125 Views
  • 1 replies
  • 0 kudos

PID PROBLEM IN CONTROLLER STM 32

Posted on August 21, 2014 at 10:02Hi,i am facing problem for the PiD controller.what parameter i have to use it for the positive & negative nos for calculation purpose.Kindly look following code New_Duty_cycle_buck=(Previous_Duty_cycle_buck + Error_...

deepak by Associate II
  • 1195 Views
  • 2 replies
  • 0 kudos

synchronous USART

Posted on August 19, 2014 at 16:38Hi everyone.I need to build a system based at STM32F4xx that use absolute encoder with BiSS protocol (http://www.biss-interface.com). This protocol is based at synchronous RS485. I have HW that convert differential ...

0690X00000602t3QAA.jpg
artuom by Associate II
  • 1593 Views
  • 2 replies
  • 0 kudos

STM32L152C6 LSE RTC WakeUp

Posted on August 26, 2013 at 09:49 Hello. I'm trying to use the RTC WakeUp feature to as a countdown timer. I've tried the code from the StdLib examples: void RTC_Config( void ) { NVIC_InitTypeDef NVIC_InitStructure; EXTI_Ini...

kaloyan by Associate III
  • 2307 Views
  • 4 replies
  • 0 kudos