STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

bit-banding GPIO->ODR not possible?

Posted on September 26, 2014 at 10:46 Hello everyone, since I'm toggling quite often some outputs, I try to access them via bit-banding. Unfortunately I can not access the GPIOs. I tested bit-banding for SRAMand RCC configuration without...

g239955 by Associate
  • 2680 Views
  • 4 replies
  • 0 kudos

STM32CubeMX NOT CREATING PROJECTS

Posted on June 01, 2014 at 07:22Hi All, I am trying to use the Cube software to generate a baseline project code. The config and manage code level is 4.2.0, and the firmware level is 1.1.0. When I step through configuring for the 429 and hit code co...

david2399 by Associate II
  • 4649 Views
  • 8 replies
  • 0 kudos

Curious behaviour of USART2 interrupt

Posted on September 26, 2014 at 10:52Hello all,I have a situation where USART2_IRQHandler is being continuously triggered.I have two control bits set, RXNIE and TXNIE, all others are set to 0.When interrupt triggers I'm checking the reason for the i...

srdjan by Associate II
  • 1028 Views
  • 3 replies
  • 0 kudos

STM32f4xx read protection problem

Posted on July 08, 2014 at 10:17Hi,I am trying to configure STM32F427 option byte to enable read out protection. I can configure it via ST-Link Utility; first I download my actual code that will run on microcontroller then I enable the read out prot...

asecen89 by Associate II
  • 879 Views
  • 1 replies
  • 0 kudos

New Software Development Studio

Posted on September 26, 2014 at 10:58Hallo. Does anybody know when STM32xxx (xxx - new software development studio integrated with STM32CubeMX end Eclipse from ST) will be released? Thanks #stm32cubemx #eclipse

giver3 by Associate II
  • 662 Views
  • 0 replies
  • 0 kudos

SPI Clock bug in STM32CubeMX V4.3.1

Posted on September 25, 2014 at 07:09For the STM32F411, I set SPI 1 as a Full Duplex Master. In the RCC Configuration, I set the VDD voltage to 3.3V. In the SPI1 Configuration, I try to set the SPI Prescaler to /2 for a Baud Rate of 50.0 MBits/s, I ...

0690X00000605S0QAI.png 0690X00000603R9QAI.jpg

PN532 NFC/RFID module with STM32F103

Posted on September 22, 2014 at 12:23Hi all.I have a project that need to connect a NFC reader/writter to STM32F103. The MCU module is designed myself so I will not mention about some modules like Arduino,...As far as I know, PN532 is a good choice ...

huonglq91 by Associate II
  • 5330 Views
  • 5 replies
  • 0 kudos

Instruction Set

Posted on September 25, 2014 at 21:49Where can I find the instruction set for the STM32F401 part? I know ... it's hardly necessary to see at all these days but I'd like to have it as a reference anyway. TIAMike #arm #joseph-yiu #assembly-instruct...

munger by Associate II
  • 1347 Views
  • 2 replies
  • 0 kudos