STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Single 0V GPIO Pulse Synched w/ Timer

Posted on October 01, 2014 at 20:31Using a STM32F427, I've got TIM5 generating an 8MHz PWM output. I've also got a GPIO output that is hooked to an active LOW enable on a device that needs to be turned on every once in awhile. What I'd like to do is...

jvavra by Associate III
  • 980 Views
  • 4 replies
  • 0 kudos

Stm32f103, hardfault problem

Posted on October 02, 2014 at 14:23Hello everyone,I've this hardfault problem for a quite long time now, I solved the issue by putting a software reset in the hardfault loop but now is not acceptable anymore.I suspect it has something to do with sen...

gnu by Associate II
  • 3184 Views
  • 2 replies
  • 0 kudos

STM32F429 discovery board USB application developpment

Posted on October 01, 2014 at 13:19Hello,I'm trying to develop a USB driver device using STM32F429 discovery board. I couldn't find any working examples that allow me to connect my board to a computer and to be detected. I would like to be detected ...

ignasi by Associate II
  • 1626 Views
  • 5 replies
  • 0 kudos

emulate EEPROM with STM32F407 flash memory

Posted on October 01, 2014 at 18:24Hi I use the routine listed below to read in flash area (sector 11) three words that contain values ​​of sampling and if the first value found is different, register the new three values. The problem is that the va...

gian0652 by Associate
  • 1273 Views
  • 2 replies
  • 0 kudos

PTP PPS output on stm32f407

Posted on September 30, 2014 at 17:07HelloI have a STM32F407ZGT6, silicon revision Z, and I'm trying to generate a 1PPS output (Pulse Per Second) on pin PG8, using the PTP. The PTP is working fine, correctly timestamping the PTP packets. In the refe...

renato1 by Associate II
  • 3412 Views
  • 5 replies
  • 0 kudos

STM32F415 read unprotect

Posted on October 02, 2014 at 08:03Hi there,I have a problem that I can't figure it out. I am coding an application that manages empty device through STM32 ROM BOOTLOADER. The problem is that when I send command for read unprotect, and check for it'...

matej2 by Associate II
  • 667 Views
  • 0 replies
  • 0 kudos

CAN TX Problem

Posted on October 01, 2014 at 19:44Hi ST Forum,Debugging a CAN TX message and can't really do it :(. I connected scope to PB13 and just see a high (3V) signal on the TX line. Anything wrong with my code below?I'm wondering if it's my CAN_mode. Can a...