User Activity

Hi all,thank you very much for the valuable advices.I am writing to you because I would like to understand how I can convert an existing program without Azure RTOS ThreadX with a program in which I use Azure RTOS ThreadX.For example I would like to a...
Hi all,I am writing to you because I am trying to understand how to make the USB CDC ACM work on the Nucleo U5A5ZJ board. First of all I analyzed some ST webinars and tested the UX_Device_CDC_ACM program which works correctly. I tried to reproduce it...
Hi all,I write to you because I would like to understand if it is really necessary to use an RTOS. I always develop projects with different ST processors (F4 and F7) without using RTOS. In those projects the F4/F7 processors communicate with many har...
Hi all,I am writing to you to find out which is the best RTOS between Azure RTOS, FreeRTOS and SafeRTOS both from the point of view of performance and from the point of view of flexibility and ease of use?I have to develop some projects with STM32U5,...
Hi all,I need to transfer big amount of data between two Nucleo U5A5ZJ-Q boards. I need to transfer a lot of data and UART communication is not sufficient, for that reason the USB HS could be the solution. I would like to test the USB HS bidirectiona...