cancel
Showing results for 
Search instead for 
Did you mean: 

CAN message

rizwin
Associate II
Posted on August 21, 2014 at 20:08

Hi,

I am trying to use CANbus on STM32F303VC6. I get it working in loopback mode. But the message is not getting sent in Normal mode. I have turned on SB21 and SB22 to connect the ports PA11 and PA12 to P2. When I debug the code, I find it getting stuck in CAN_TransmitStatus() function due to pending message. Please point out what might be the problem.

#include ''stm32f30x.h''

#include ''stm32f3_discovery.h''

#include ''stm32f30x_it.h''

#include ''stm32f30x_rcc.h''

#include ''stm32f30x_can.h''

#include ''stm32f30x_gpio.h''

#include ''stm32f30x_misc.h''

#include ''CAN.h''

void Init_TxMes(CanTxMsg *TxMessage){

          /* Transmit INITIALIZATION*/

     TxMessage->IDE = CAN_ID_STD;

     TxMessage->DLC = 2;

     TxMessage->StdId = 0x321;

     TxMessage->RTR = CAN_RTR_DATA;

}

void Init_RxMes(CanRxMsg *RxMessage)

{

  uint8_t i = 0;

  RxMessage->StdId = 0;

  RxMessage->IDE = CAN_ID_STD;

  RxMessage->DLC = 0;

  RxMessage->FMI = 0;

  for (i = 0; i < 8; i++)

  {

    RxMessage->Data[i] = 0;

  }

}

void CAN_setup(void)

{

    NVIC_InitTypeDef NVIC_InitStructure;

    RCC_APB1PeriphClockCmd(RCC_APB1Periph_CAN1, ENABLE); //Enable the clock for CAN

    RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);    

    

    GPIO_PinAFConfig(GPIOA, GPIO_PinSource11 | GPIO_PinSource12 , GPIO_AF_9);   

    

    /* Configure CAN1 RX pin */

   GPIO_InitStructure.GPIO_Pin = GPIO_Pin_11;

   GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;

   GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;

   GPIO_Init(GPIOA, &GPIO_InitStructure);

    

        /* Configure CAN1 TX pin */

     GPIO_InitStructure.GPIO_Pin = GPIO_Pin_12;

     GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;

     GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

     GPIO_InitStructure.GPIO_PuPd  = GPIO_PuPd_NOPULL;

     GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

     GPIO_Init(GPIOA, &GPIO_InitStructure);

    

    /* Enable the CAN global Interrupt */

    NVIC_InitStructure.NVIC_IRQChannel = CAN1_SCE_IRQn;

    NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;

    NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1;

    NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

    NVIC_Init(&NVIC_InitStructure);

    

    NVIC_InitStructure.NVIC_IRQChannel = CAN1_RX1_IRQn;

    NVIC_Init(&NVIC_InitStructure);

    

     CAN_DeInit(CAN1);

     /* Configure CAN1 **************************************************/  

     /* Struct init*/

   CAN_StructInit(&CAN_InitStructure);

   CAN_InitStructure.CAN_TTCM = DISABLE;

   CAN_InitStructure.CAN_ABOM = DISABLE;

   CAN_InitStructure.CAN_AWUM = DISABLE;

   CAN_InitStructure.CAN_NART = DISABLE;

   CAN_InitStructure.CAN_RFLM = DISABLE;

   CAN_InitStructure.CAN_TXFP = ENABLE;

   CAN_InitStructure.CAN_Mode = CAN_Mode_Normal;  

   CAN_InitStructure.CAN_SJW = CAN_SJW_1tq;  

   CAN_InitStructure.CAN_BS1 = CAN_BS1_3tq;

   CAN_InitStructure.CAN_BS2 = CAN_BS2_2tq;

   CAN_InitStructure.CAN_Prescaler =6;

     /*Initializes the CAN1 */

   CAN_Init(CAN1,&CAN_InitStructure);

    

    

   /*CAN1 filter init */

   CAN_FilterInitStructure.CAN_FilterNumber = 1;

   CAN_FilterInitStructure.CAN_FilterMode = CAN_FilterMode_IdMask;

   CAN_FilterInitStructure.CAN_FilterScale = CAN_FilterScale_32bit;

   CAN_FilterInitStructure.CAN_FilterIdHigh = 0x6420;

   CAN_FilterInitStructure.CAN_FilterIdLow = 0x0000;

   CAN_FilterInitStructure.CAN_FilterMaskIdHigh = 0x0000;

   CAN_FilterInitStructure.CAN_FilterMaskIdLow = 0x0000;

   CAN_FilterInitStructure.CAN_FilterFIFOAssignment = 0;

   CAN_FilterInitStructure.CAN_FilterActivation = ENABLE;

   CAN_FilterInit(&CAN_FilterInitStructure);

 

}

int main (void)  {

  int i;

  uint8_t TransmitMailbox = 0;

  CAN_setup ();                                   // setup CAN interface

  Init_TxMes(&TxMessage);

    while(1){

         TxMessage.Data[0] = 0xAB;

         TxMessage.Data[1] = 0xCD;

        TransmitMailbox = CAN_Transmit(CAN1,&TxMessage);

        i = 0;

        while((CAN_TransmitStatus(CAN1, TransmitMailbox) != CANTXOK) && (i != 0xFF)) // I put a breakpoint here to check and found the message is pending

            i++;

    }
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Posted on August 21, 2014 at 20:56

And you have this connected to a transceiver, and another CAN receiver? ...

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
rizwin
Associate II
Posted on August 22, 2014 at 10:39

Yes. I have it connected to a bus sniffer, PCAN-View.

rizwin
Associate II
Posted on August 22, 2014 at 12:46

Found the problem... When the GPIO_PinAFConfig() is done after GPIO_Init(), it started working!!

  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_11 | GPIO_Pin_12;

  GPIO_InitStructure.GPIO_Mode  = GPIO_Mode_AF;

  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

  GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

  GPIO_InitStructure.GPIO_PuPd  = GPIO_PuPd_UP;

  GPIO_Init(GPIOA, &GPIO_InitStructure);

    

  GPIO_PinAFConfig(GPIOA, GPIO_PinSource11, GPIO_AF_9);

  GPIO_PinAFConfig(GPIOA, GPIO_PinSource12, GPIO_AF_9);