STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Do you use STM32cubeMX

Posted on November 19, 2014 at 19:39Hello,ST announced that everybody should use the cubeMX software (or at least libraries) because the old libraries will not be supported anymore. I was a noob on STM32 so I decided to start with cubeMX.It it clear...

tarzan2 by Senior
  • 2154 Views
  • 6 replies
  • 0 kudos

sdio fatfs speed problem

Posted on January 22, 2014 at 20:31i use fatfs and i read at about 200to300KB/SECOND  it's very low speed . i test sd card speed from computer and it's speed reading 12.5MB/SECOND how to speed up sd card reading i want about 5MB/sec are this hard ...

elec_st by Associate III
  • 4649 Views
  • 25 replies
  • 0 kudos

STM32L0xx Altium Files

Posted on November 20, 2014 at 16:44Hi, Are STM32L0xx files (sch, lib, ref design) for Altium Designer available somewhere for download? In order to go quickly and avoid error..... Thanks

STM32F407: Strange Idle/RXNE on UART4-5 (not on USART1-3/6)

Posted on November 20, 2014 at 12:30Hi, I found a very strange behaviour for the UARTs: The IDLE Flag of UART4-5 will ''extinguish'' after typically 100-500msec (Baudrate 100kB and 9600). I tried with 2 Discovery boards and with all UARTs. The ''sy...

flyer31 by Senior
  • 1043 Views
  • 3 replies
  • 0 kudos

volatile variables and ''functions''

Posted on November 20, 2014 at 11:48 Hello, i am running compile (IAR AMR) in highest optimization settting, but sometimes it does ignores my code, or even functions that does have purpose; as example, DataRx[] is loaded by DMA with ...

Nucleo STM32F334R8 DAC

Posted on October 23, 2014 at 14:05Hello community,Actually I evaluating DAC on NucF334R8. DAC1_Channel1 seems to work but I am not able getting DAC2_Cannel1 (Pin PA6) to work. I created the C Framework with STMCubeMX 4.4.0 - both channels with equa...

0690X00000605OxQAI.png
heap by Associate II
  • 4402 Views
  • 13 replies
  • 0 kudos

STM32F429 - Erase falsh sector doupts

Posted on November 20, 2014 at 11:38Hi,I am using STM32f429 disco FW_upgrade code as bootloader for my application. I had seen it erase only 11 sectors (1MB) of flash memory. I want to erase upto 23 sectors from my application address, So i have mod...

STM32F103VCT6 CAN Bit timing settings

Posted on November 18, 2014 at 14:54I am using STM32F103VCT6 controller in one of our product and we need to configure CAN bit timings to work at 125KBPS, 250KBPS and 500KBPS at clock frequency of 36MHz (max system clock on bus). I need to know two ...

Cubemx 4.3.1 download location

Posted on November 05, 2014 at 06:52Hello. Where can I download the cubemx 4.3.1 version? The 4.4.0 has bugs with code generation in my project.

totti001 by Associate II
  • 1039 Views
  • 1 replies
  • 0 kudos

STM32F0 internal bootloader mode

Posted on November 19, 2014 at 23:48Hi All,   I would like to jump to the internal bootloader mode from my application code.Previous research on this topic in this forum suggested not to directly jump to the system memory from the application code b...