cancel
Showing results for 
Search instead for 
Did you mean: 

DMA SDIO TX underrun error

zeros_and_ones1991
Associate III
Posted on March 08, 2014 at 14:46

I got the DMA working fine with SDIO , i can read multiple blocks ok , but when i try write multiple blocks , i get TX underrun error in the SDIO , and i can also see that there is a FIFO error in the DMA , which i do not see when reading from the card ......... any suggestions ?

#lmgtfy:-firmware-library
This discussion is locked. Please start a new topic to ask your question.
7 REPLIES 7
Posted on March 08, 2014 at 15:40

Have you reviewed ST's implementation for SDIO?

Writing is a little more problematic than reading, there are two FIFO's, one in the DMA, and one in the SDIO (128 Byte 32x4). It's important to wait for the SDIO to empty before the command actually completes, and this can be some time after the DMA TC. The FIFO on the DMA side is likely it be sensitive to settings size/alignments, and the alignment/bandwidth of the data.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
zeros_and_ones1991
Associate III
Posted on March 08, 2014 at 15:50

I Know what u saying clive , but im not using the FIFO of the DMA , and i do not think i should have problem with the FIFO of SDIO , cuz im making the SDIO as the flow controller , ........ where is this documentation u r talking about ? ....... and Have u encountered that problem ? ..... what do u suggest ?

Posted on March 09, 2014 at 01:41

IMPLEMENTATION != DOCUMENTATION.....Review something that works.....Conveys details, nuances and methods which are hard to express by a technical writer who didn't design/work with the silicon/software....Not using FIFO mode for the DMA?..... Perhaps you should be using FIFO/BURST mode if you understood the tight delivery deadlines, and reviewed other solutions.....What's the SDIO peripheral supposed to do with the clock signal if the delivery of data stalls out?.....Does the throttling occur at a block level?.....Underrun, doesn't that infer an inability of your data source to supply it sufficiently rapidly when it needs too?

STM32F4xx_DSP_StdPeriph_Lib_V1.3.0\Project\STM32F4xx_StdPeriph_Examples\SDIO\SDIO_uSDCard

STM32F4xx_DSP_StdPeriph_Lib_V1.3.0\Utilities\STM32_EVAL\STM3240_41_G_EVAL\stm324xg_eval_sdio_sd.c

STM32F4xx_DSP_StdPeriph_Lib_V1.3.0\Utilities\STM32_EVAL\STM3240_41_G_EVAL\stm324xg_eval.c
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Amel NASRI
ST Employee
Posted on March 10, 2014 at 13:30

Hi Muhammad,

In

http://www.st.com/web/en/resource/technical/document/application_note/DM00046011.pdf

, there is a note saying the following:

If the user enables the used peripheral before the corresponding DMA stream, a “FEIF�?

(FIFO Error Interrupt Flag) may be set due to the fact the DMA is not ready to provide the first required data to the peripheral (in case of memory-to-peripheral transfer).

Check if you are in similar case.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

ta
Associate II
Posted on May 13, 2014 at 14:45

Hi. Can you add link for the last STM32 STD Lib (1.3)? I try to find it on my.st.com without success.

Posted on May 13, 2014 at 15:38

http://www.st.com/web/en/catalog/tools/PF257901

Google search terms ''stm32f4 dsp firmware''
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
ta
Associate II