2014-04-03 6:13 PM
Does anyone have an .ioc file that can be used as a base project in STM32CubeMX to generate a project for STM32F429ZIT DIscovery evaluation board ?
ThanksKartik #discovery #stm32f4 #exti2014-04-03 11:45 PM
I've been asking for the same this in my posts about 3 weeks earlier, but without any luck from ST.
2014-04-04 1:43 AM
Hi Kartik,
Are the files attached to what you are looking for? Nic D, What I understood from your request in is that you are looking for IOC files related to eval board, not discovery one, isn't the case? -MaylaTo give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2014-04-04 10:54 AM
2014-05-13 4:47 AM
Hi Mayla,
Exactly! Is there anyway I can get the IOC file for the evaluation board?Thanks,Nicholas2014-05-13 5:05 AM
When you start CubeMX, click ''New Project'' and click ''Board Selector''. There is an entry for the STM32F429-Discovery Board.
2014-05-13 5:09 AM
2014-05-15 6:40 AM
Ahh... this must have been a new addition, as this tab didn't exist in the original release of STM32CubeMX.
I see the IOC for the STM32F429I-Eval has the ethernet disabled, but the actual evaluation PCB (which I have on my desk) has it very much enabled and running and using LWIP - so am a bit confused as to what this file is representing. Any ideas?From: skibowski.klaus.001Posted: Tuesday, May 13, 2014 2:09 PMSubject: Is there an STM32CubeMX Configuration for the STM32F429 Discovery boardsorry, should be ''STM32F429I-Eval''.