STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F07xx: Behaviour if internal flash is corrupted

Posted on February 05, 2015 at 14:05Hi all, how does the STM32 behaves during a power-on start-up if the flash is corrupted? Does it enters the boot mode again to try the USB DFU again, do I have to reanimate with a debugger, ... ? This condition ma...

stm32f103 clock (RCC) problem

Posted on February 05, 2015 at 12:42Hi all,i'm working on 103 MCU. first step is to bring up the 72Mhz clock.problem is i'm able to get clock upto 64Mhz (tested with systick),but when i configure pll mul factor to 9 control is moving to default hand...

Start two timers synchronous in STM32F1 eval board

Posted on February 05, 2015 at 06:30Hello,I have to start two timers exactly at the same time... like In my program i am using TIM3 four channels for 4 four hall sensors and TIM4 for 5 hall sensor... I need to start all the 5 hall sensors at time.. ...

santhosh by Associate
  • 1166 Views
  • 1 replies
  • 0 kudos

STM32F2 and two nand targets

Posted on February 05, 2015 at 05:09Hi, I'm working on a board that interfaces an STM32F2 with a 4GB nand flash from Micron MT29F32G08AFABAWP:B. That nand flash is split up internally to two different dies. They use most of the same data and control...

Bug in STM32cube HID code for STM32F103

Posted on February 01, 2015 at 23:22I just started playing with the USB code for the stm32f103c8.  I found it quite impressive.  It was the only tool I tried so far that was able to produce working code for a HID device that enumerated properly.  Ho...

h500ca by Associate
  • 1075 Views
  • 1 replies
  • 0 kudos

Stm32 StdPeriph driver and Eclipse CDT configuration

Posted on February 04, 2015 at 22:57Hi guys! I have a problem with my stm32 discovery board. I installed eclipse, gnu arm plugin(version 2.2.1), gcc arm none eabi(4_9-2014q4).I did not install latest gnu arm plugin because i don't want to use hal_dr...

Nucleo L053 & IDB04A1 & IDB002V1

Posted on December 24, 2014 at 03:02We're looking to evaluate the Nucleo STM32L053 with the BlueNRG shield.  On hand, we also have the IDB002V1 eval kit for the BlueNRG.We're following the documentation in AN4559 to evaluate the SensorDemo program. ...

eleventen by Associate III
  • 996 Views
  • 2 replies
  • 0 kudos

Which CubeMX packages should be installed?

Posted on January 26, 2015 at 23:25Are the cube firmware packages cumulative? Version STMCubeF4 1.4.0 came out recently, but I noticed that version 1.2.0 is significantly smaller than 1.1.0 or 1.3.0. This hints that all of the packages should be ins...

STM32L - can't change Brownout level

Posted on January 26, 2015 at 11:25 Hey there, today i wanted to change the brownout level from 1 to 4, but i failed. I'm using the STM32L151VDT6 and the following code at startup if ((FLASH_OB_GetBOR() & 0x0F) != OB_BOR_LEVEL...

juergen23 by Associate II
  • 2454 Views
  • 3 replies
  • 0 kudos