Posted on December 29, 2016 at 14:58Hello,I use ST-Link Utility v4.0.0 and STM32F103RC.CommandST-LINK_CLI.exe -c SWD -OB RDP=1gives message 'could not update the option bytes' but option bytes updated. And command returns an error code.GUI gives the...
Posted on November 12, 2016 at 23:43I use STM32CubeMX 4.17.0. I create a new project and select any F1. Then, I generate a source code. In function HAL_MspInit() I see following lines: /**DISABLE: JTAG-DP Disabled and SW-DP Disabled */ __HAL...
Posted on June 28, 2014 at 11:30There is equation in AN4013 timer overview:CCx update rate = TIMx_Counter_CLK / CCRx.What is CCx update rate?Does CCx update rate depend on ARR? #timer #an4013
Posted on October 18, 2012 at 11:15In STM32F10x Standart Peripherals Library v3.5.0, stm32f10x.h, line 3616:&sharpdefine DMA_CCR7_PSIZE , ((uint16_t)0x0300)Not needed comma? #stm32f10x-spl #error