SPI Problem in STM32F215
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2014-06-28 8:42 AM
Posted on June 28, 2014 at 17:42
Hi,
I have written code for configuration and Data_send for SPI in stm32f215 like below mentioned code. I have monitor the clk,data,CS while running using CRO, i am getting CLK,Data but not getting CS. What is the problem please clear me. Below is code. int main() { SPI_Config(); while() { SPI_I2S_SendData( SPI1, 0x55); } } static void SPI_Config(void) { GPIO_InitTypeDef GPIO_InitStructure; NVIC_InitTypeDef NVIC_InitStructure; /* Peripheral Clock Enable -------------------------------------------------*/ /* Enable the SPI clock */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_SPI1, ENABLE); /* Enable GPIO clocks */ RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE); /* SPI GPIO Configuration --------------------------------------------------*/ /* Connect SPI pins to AF5 */ GPIO_PinAFConfig(GPIOA, GPIO_PinSource4, GPIO_AF_SPI1); GPIO_PinAFConfig(GPIOA, GPIO_PinSource5, GPIO_AF_SPI1); GPIO_PinAFConfig(GPIOA, GPIO_PinSource6, GPIO_AF_SPI1); GPIO_PinAFConfig(GPIOA, GPIO_PinSource7, GPIO_AF_SPI1); GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_DOWN; /* SPI SCK pin configuration */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4; GPIO_Init(GPIOA, &GPIO_InitStructure); /* SPI MOSI pin configuration */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_5; GPIO_Init(GPIOA, &GPIO_InitStructure); /* SPI SCK pin configuration */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6; GPIO_Init(GPIOA, &GPIO_InitStructure); /* SPI MOSI pin configuration */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_7; GPIO_Init(GPIOA, &GPIO_InitStructure); /* SPI configuration -------------------------------------------------------*/ SPI_I2S_DeInit(SPI1); SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex; SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b; SPI_InitStructure.SPI_CPOL = SPI_CPOL_Low; SPI_InitStructure.SPI_CPHA = SPI_CPHA_1Edge; SPI_InitStructure.SPI_NSS = SPI_NSS_Soft; SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_2; SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB; SPI_InitStructure.SPI_CRCPolynomial = 7; /* Configure the Priority Group to 1 bit */ NVIC_PriorityGroupConfig(NVIC_PriorityGroup_2); /* Configure the SPI interrupt priority */ NVIC_InitStructure.NVIC_IRQChannel = SPI1_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 1; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); SPI_InitStructure.SPI_Mode = SPI_Mode_Master; SPI_Init(SPI1, &SPI_InitStructure); /* The Data transfer is performed in the SPI interrupt routine */ /* Enable the SPI peripheral */ SPI_Cmd(SPI1, ENABLE); } Regards, Thirukkannan.P
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2014-06-28 9:31 AM
Posted on June 28, 2014 at 18:31
Probably not a SOFT control of CS then? Doesn't that imply it's a GPIO?
The loop should also wait on TXE before jamming data out.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Up vote any posts that you find helpful, it shows what's working..