STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

[SOLVED] stm32f0 discovery board as debugger

Posted on February 23, 2015 at 23:15 Hi everyone! I am using st-link on stm32f0 discovery board and ST-LINK utility to program some other boards and that is working like it should. I am working with stm32f030 processor. I am wond...

zlajoan by Associate II
  • 1443 Views
  • 2 replies
  • 0 kudos

USB devices with 2 interfaces.

Posted on June 19, 2014 at 18:02Hi guys, looking for some help with a USB device I have which has 2 interfaces. The first interface is HID, and the second is MSC. I've modified the USB Host library so that it doesn't it doesn't fail in the MSC Inter...

STM324x9I-Eval : Trace Configuration

Posted on February 23, 2015 at 23:53Hello everyone,I juste received an ulinkpro so I can use the ETM feature later on in my development.  Right now, I am trying to simply display a variable in the logic analyzer but I get no synchronization.  I read...

keaven by Associate II
  • 1225 Views
  • 3 replies
  • 0 kudos

external sdram connection to stm32f429ii

Posted on December 05, 2014 at 19:19Hi,i'd like to connect an external sdram to stm32f429ii controller. There is a question, is it necessary to use dqm pins?  i want to use MT48LC4M32B2 sdram.

Quadrature Encoder STM32 Z Capture

Posted on February 23, 2015 at 15:03 Hello,I'd like to use an quadrature encoder connected to my STM32F4 Discovery Board.I have connected the A and B outputs to PC6 and PC7. CH1 and CH2 of TIM8.It works pretty good, the timer counts.Now I'd like to...

arapp1990 by Associate II
  • 1811 Views
  • 2 replies
  • 0 kudos

SPI Software Chip Select

Posted on February 14, 2015 at 13:46 What is the best way to implement chip select in software? I've tried doing it this way: HAL_GPIO_WritePin(NSS_PORT, NSS_PIN, GPIO_PIN_RESET); HAL_SPI_Transmit(&hspi1, out , 1); HAL_GPIO_WritePin(NSS_P...

dscdsc by Senior
  • 3263 Views
  • 5 replies
  • 0 kudos

Update Binary with Bootloader

Posted on February 23, 2015 at 16:29Hello,I´m trying to update my application with the Preprogramed bootloader by apropiate uart and pins BOOT1/0 according to that task.I could use this application to do that, couldnt I?My Keil compilation makes 2 f...

0690X000006030NQAQ.jpg 0690X000006030SQAQ.jpg
gerardo by Associate II
  • 1496 Views
  • 2 replies
  • 0 kudos

Poblem programming stm32f334 witn the flash loader demo 2.7.0

Posted on February 19, 2015 at 09:09I can program the stmf32f334 chip without problem with the  desktop version ''FlashLoaderDemo.2.7.0'' - it is Ok. But the command line version gives error: ''The instruction of ''0x7c911699'' referenced memory of ...

var2 by Associate III
  • 1849 Views
  • 3 replies
  • 0 kudos

5 V pulse board stm32f407

Posted on February 19, 2015 at 16:28Hello, i want to generate a periodic pulse of 5V into a pin using a TIMER. Has someone a code similar to this? Thank you #timers #stm32f4 #stm32f407 #discovery

fiulala by Associate II
  • 1256 Views
  • 2 replies
  • 0 kudos

Will STM32F407ZG supports using AS1115 driver ?

Posted on February 23, 2015 at 10:33I am having a custom board with STM32407ZG, the board also has AS1115 driver IC for supporting the keypad and led lights. Is there any example relating to this combo? #stm32f407zg #- #as1115 #example

dhinesh by Associate
  • 950 Views
  • 1 replies
  • 0 kudos