STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

emWin Problem on DROPDOWN_SetItemDisabled function

Posted on April 10, 2015 at 09:37I have discovered that DROPDOWN_SetItemDisabled function always crash with emWin V5.22I found the it has been solve with version 5.24BCurrently, NXP's support emWin V5.24B So, ST does have any plan to update emWin li...

Standard Peripheral Library Documentation

Posted on April 09, 2015 at 17:51Hello,I'm using the standard peripheral library for the STM32F4discovery at the moment because in Cube, there are too many bugs at the moment and so it's currently unuseable for me.When downloading the standard perip...

stop, standby mode with ADC

Posted on April 10, 2015 at 06:49Hi all,When I using ADC it work correctly, but when I want MCU enter STOP(or standby) mode and wakup by external interrupt, ADC is hang, can not convert ADC./**  ******************************************************...

np1 by Associate II
  • 1103 Views
  • 1 replies
  • 0 kudos

STM32F401: how to control a TFT display

Posted on April 08, 2015 at 17:26Hello everybody, I'm evaluating STM32F401 and other MCU to control a TFT display. There is no need to send pixel data at fixed speed, TFT display has a driver with internal RAM which manages syncs, porchs, pixel cloc...

stm32f07+touch

Posted on April 09, 2015 at 17:40hello every onei want to connect touch panel to the adc of stm32f0 directlyso i use PA3->X+ PA4 ->Y+PA5->X-PA6->Y-pa5,pa6 just use as gpio and pa3,pa4 use as gpio and adc bothi config the adc first and defult channel...

Starting SPI master with DMA by an external signal

Posted on April 03, 2015 at 18:02I'm trying to read the serial data from two AD7766 (24 bit ADC in daisy chain mode) with a STM32F4 discovery board. The two AD7766 generates every 8 us new data. This is indicated by the ''Data Ready'' (DTRY) pin who...

freddy by Associate II
  • 1604 Views
  • 2 replies
  • 0 kudos

syscalls.c & uart.c

Posted on April 09, 2015 at 01:39Using gcc compiler with stm32f407 device FreeRTOS based FAT32 file system, Moment I remove uart.c and uart.h whole program halts nothing works. very strange its third day in debugging. Attached syscall.c and syscalls...

DMA request queue

Posted on April 09, 2015 at 06:10Hi all,I am working on an STM32F0 project in which I am triggering a DMA transfer using peripheral events such as an input capture. Looking over the docs it seems a little vague as to the behaviour of the DMA control...

luke2 by Associate II
  • 2002 Views
  • 2 replies
  • 0 kudos

STM32F4-DIscovery FAT example wrong

Posted on April 07, 2015 at 12:52In example:if(f_open(&MyFile, ''STM32.TXT'', FA_CREATE_ALWAYS | FA_WRITE) != FR_OK) Keil output: error:  &sharp167: argument of type ''char *'' is incompatible with parameter of type ''const TCHAR *''        if(f_ope...

chief by Associate II
  • 2539 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.