STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Stm32F429I-Discovery Board stm32cubef4\STM32Cube_FW_F4_V1.5.0\Projects\STM32F429I-Discovery\Demonstrations_ Example

Posted on May 09, 2015 at 14:25i am using this example  stm32cubef4\STM32Cube_FW_F4_V1.5.0\Projects\STM32F429I-Discovery\Demonstrationsi want to change the Icons in the Demo Applicationwhat type of Tool am i required to convert bmp to c fileHere the...

senthil by Associate II
  • 904 Views
  • 2 replies
  • 0 kudos

DMA connections in stm32f103c8

Posted on May 10, 2015 at 07:31Helloaccording to it's datasheet and reference manual, only DMA1 controller is active in this device.Is GPIO peripheral connected to DMA streams in this device so that GPIO to memory transfers can be implemented?Thanks...

Startup Files with different chipsets

Posted on April 20, 2015 at 23:28Hi all,I have a legacy boot loader that was run on an STM32F407.  It was located at 0x08000000 and my main application is located at 0x08020000.  I have seen a strange behaviour when I compile my main application cod...

FSMC do not work

Posted on May 10, 2015 at 07:08I crate a project with stm32cube my chip is stm32f103zc i enable fsmc for lcd interface and 16 bit data address and A0 for register select . this function HAL_SRAM_Read_16b(&hsram1,&send_address,send_buffer,10); do no...

USB soundcard reference design

Posted on May 10, 2015 at 08:48Hi All I want to use the F429 as a USB soundcard  for a windows pc. with Both Inputs (Mic) and outputs(speaker) Only need 16khz 16bit sample rates. I cannot appear to find  any ST reference designs I have heard about t...

brett23 by Associate II
  • 954 Views
  • 0 replies
  • 0 kudos

STM32CubeMX + MDK-ARM: retargeting printf output

Posted on November 25, 2014 at 01:21Hi All,I'm using the tools as per the subject.Can you advise how I can configure printf to trace to a serial terminal?Currently I'm using a Nucleo board (Nucleo L053R8) but soon I'm moving on to Discovery (STM32F4...

balazs by Associate II
  • 1697 Views
  • 3 replies
  • 0 kudos

comparator output as tim15 IC1 and TRGI

Posted on May 09, 2015 at 13:25I'm using analog hall sensor in my application. One of its tasks is to measure rpm. I also calculate angle, so it's connected to ADC input + I internally connected it to COMP3-. Comp out, if I pass it to PA8 looks ok. ...

tov by Associate II
  • 1690 Views
  • 4 replies
  • 0 kudos

STM32F4 discovery GPIO remapping

Posted on May 08, 2015 at 22:22Hi everyone from London in the UK.My name is Steve. I have an STM32 F4 discovery board and am attempting to get I2S and the audio codec working for the STM32Duino project. The project is the brainchild of Roger Clark f...

defacato by Associate II
  • 1779 Views
  • 2 replies
  • 0 kudos

stm32f4: issues with rts/cts flow control with UART

Posted on May 09, 2015 at 03:07 I am trying to get RTS/CTS working with UART3. I am using theMCBSTM32f400 (STM32F407VG) board and connected a serial cable on the UART3 with a PC. If i am not using the flow control on the PC side, i can ge...

abhiran by Associate
  • 1336 Views
  • 1 replies
  • 0 kudos