STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

input capture mode

Posted on June 05, 2015 at 11:29hej, i am getting a wrong values when i measuring the signal in input capture mode.can anyone help me what i am doing wrong and also i am new to this .i am using stm32f407vg the below oen is intialization. /new one  ...

arunl4g by Associate II
  • 2235 Views
  • 5 replies
  • 0 kudos

FM24C256 FRAM programming (STM32F0xx-DISCOVERY Board)

Posted on June 03, 2015 at 09:42 Hello dear members of forum, I would like to use a FM24C256 ram of RAMTRON ( http://www.kosmodrom.com.ua/data/memory/FM24C256ds_r3.1.pdf). I have tryed to write program for it but It do not work. When I...

STM32F407 SPI TXE flag Interrupt problem.

Posted on June 04, 2015 at 11:53Hi, I am using the STM32F407 SPI TXE and RXNE interrupts. The ISR checks if there is data to transmit or if any data is received. The data to be transmitted is filled outside the ISR and the TXE interrupt and CS is en...

abhisheke by Associate II
  • 2738 Views
  • 5 replies
  • 0 kudos

SPI_HandleTypeDef structure extern?

Posted on June 05, 2015 at 00:09I've used CubeMX to init SPI. There is a struct called hspi3 created by the init code which holds settings for SPI. I would like to use SPI library in a C file I've written (DAC driver) but I can't because HAL_SPI_Tra...

GPIO port on fly selection mechanism in stm32f4xx

Posted on June 05, 2015 at 09:41HelloIf i want to connect output of an ADC(analog to digital converter) to two different ports, e.g. GPIOA and GPIOB, and to modify this selection by means of software code(no hardware modification needed), how is it ...

STM32F407 Discovery board to control bldc

Posted on June 05, 2015 at 18:28I am looking at implementing a 3 phase BLDC using hall sensor inputs and motor commutation on timers on the discovery 407 board. I have reference of http://www.mikrocontroller.net/articles/STM32_BLDC_Control_with_HAL...

gmali9 by Associate
  • 866 Views
  • 0 replies
  • 0 kudos

Problem with getting job

Posted on June 05, 2015 at 10:07Hello dear friends ! I working for freelance programmer microcontroller about 1 year . Today, I want to get formal employment in some companies . But employers are not interested in a freelance programmers , everyone ...

bomon85 by Associate
  • 1159 Views
  • 2 replies
  • 0 kudos

CCM and Structures

Posted on June 05, 2015 at 16:07 Hi everyone, I need to put the maximum of my data in the CCM. This is already done for simple types like this : uint32_t memory_dur_init __attribute__ ((section( ''.ccm'' ))); I'm scratching my h...

benoit2 by Associate II
  • 1024 Views
  • 1 replies
  • 0 kudos