cancel
Showing results for 
Search instead for 
Did you mean: 

DMA transfer (Reception) not proper when implemented with ethernet communication

arunnmishra
Associate II
Posted on November 24, 2014 at 07:54

Hello there,

I am using Lwip library for Ethernet implementation. I poll for the Ethernet packet in main loop. Then the packet is passed to further libraries to process it. 

Meanwhile I have also to receive 8 bit data on Port GPIOH  with clock on Timer 8 capture. Using DMA2, channel 7. 

Receiving 220 bytes of parallel  data @20 Mhz. DMA transfers it from GPIO port H to internal RAM

If I run the DMA without ethernet, it runs perfectly fine. but when ethernet is switched on, some of the DMA packets are lost.

Did a test and found 400 packets out of 100000. (0.4%)

Do not have sufficient window to retransmit the packet. 

But cannot afford to loose the packet.

Hardware issues like noise etc are ruled out. Please Help.

Thanks in advance

#stm32f4 #dma
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
waclawek.jan
Super User
Posted on November 24, 2014 at 15:24

You didn't say which chip, but try to place the ethernet buffers and the DMA target into different SRAM.

JW