STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Scheduling future interrupts with a specific delay

Posted on July 09, 2015 at 01:12I'm trying to schedule a single interrupt in the future with a specific delay on the STM32F407, and I'd like to figure out the best way of doing this. I've played around with periodically waking up a task and generati...

Timer 8 of STM32F4 Discovery don't work !

Posted on March 11, 2013 at 10:54Hi,I have problems with Timer 8 this time. I want to measure the frequency of an input signal. I have to use PB1 that's connected to TIM8_CH3N. The code seem correct but it doesn't give any frequency. The code is the...

DSP functions on System Workbench and CubeMX

Posted on July 04, 2015 at 15:46 Hi, I'm trying to setup a project using System Workbench and CubeMX on an Nucleo Board (411RE). Could someone tell me a step by step on how to do that? I have an example fromSTM32Cube\Repository\STM32Cube_F...

stm32f0 discovery board to run One Pulse Mode on timer 2

Posted on July 09, 2015 at 22:13Hi, I am using the discovery board to try OPM on timer 2. I can not get it going with any effort on my code list below. Please help!!! It is important to our new product.void GPIO_Configuration(void);int main(void){  ...

ming2 by Associate III
  • 1967 Views
  • 5 replies
  • 0 kudos

I2C problems with STM32L Discovery

Posted on July 10, 2015 at 18:25I am trying to communicate with a ADT7410 I2C temperature sensor using a STM32L Discovery Board (PB6 for SCL and PB7 for SDA).I configure the I2C with the following code:void I2C_initialization(void){  I2C_InitTypeDef...

Baud Rate problem

Posted on July 09, 2015 at 17:15  The original post was too long to process during our migration. Please click on the attachment to read the original post.

fiulala by Associate II
  • 1260 Views
  • 4 replies
  • 0 kudos

Stop code execution during 8 timer interrupts

Posted on July 03, 2015 at 14:14Hi everyone, I'm working with the stm32f405 microcontroller and I am trying to send some characters using a simple GPIO pin. My problem is that I have to send each bit of one character every 20ms. For that I use a ti...

mnemxys by Associate II
  • 1418 Views
  • 2 replies
  • 0 kudos