STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

St-link Error in HEX parser

Posted on April 23, 2015 at 18:22Hi folks!I found a serious error in the ST-Link v3.6 parser.I have a project with the https://launchpad.net/gcc-arm-embedded 4.9-2014q4 toolchain.It generates a valid intel hex file, whit the small quirk, that there ...

0690X0000060316QAA.jpg
rigomate2 by Associate III
  • 3023 Views
  • 3 replies
  • 0 kudos

ST-Link Utility HEX bug ?

Posted on June 19, 2015 at 19:15Hi All Using ST-Link 3.6.0 to download a HEX file to an STM32F407 board I found that the loaded code sometimes didn't run. But, if I loaded the BIN version instead it was OK. After some investigation I found that the ...

hpipon957 by Associate III
  • 2566 Views
  • 7 replies
  • 0 kudos

ST Link Utility 3.7

Posted on July 11, 2015 at 08:18Hi to all,According to the release notes of ST Link Utility, the latest release is 3.7. This release supports STM32F7x development boards (like the discovery one). But, at the moment it's possibile to download only th...

carmine by Associate II
  • 2850 Views
  • 8 replies
  • 0 kudos

FreeRTOS with CubeMX different than freertos.org

Posted on July 29, 2015 at 19:15There seem to be many differences between FreeRTOS code generated with CubeMX, and FreeRTOS code examples downloaded from freertos.orgI use the ''Prectical Guide'' and Example code from freertos.org, but have to modif...

gerhard by Associate II
  • 2066 Views
  • 2 replies
  • 0 kudos

STM32F103 Virtual Com Port problem

Posted on July 30, 2015 at 17:55 Hello I have been trying to implement the VCP on a chip I am working on. I do not have any experience with USB and I just want to get this working so I can send some data to the device (will focus on USB ...

tbnkr by Associate II
  • 940 Views
  • 0 replies
  • 0 kudos

STM32F3 16-bit SD ADC resolution in Single Ended mode.

Posted on July 25, 2015 at 13:19I would like to know what is the maximal resolution of 16-bit Sigma Delta ADC on STM32F3 line of microcontrollers when used in single ended mode? Can it achieve full 16-bit resolution, 0-65535, in SE mode?

milanmeh by Associate
  • 888 Views
  • 1 replies
  • 0 kudos

Cube F4 V1.7.0, Timer interrupt macros

Posted on July 30, 2015 at 14:19 Hello Is there a specific reason that the timer interrupt macros for clear flag (and respectivly clear interrupt since they are the same) don't have an &= operator? #define __HAL_TIM_ENABLE_IT(...

Hal driver error 258

Posted on July 17, 2015 at 12:48Hello, A few days ago I started my adventure with stm32 microcontrollers. To be able to programm them easly I downloaded CubeMX  from this side http://www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1533/PF259242?sc...

dooz by Associate II
  • 1851 Views
  • 3 replies
  • 0 kudos

STM32F303 ADC clocks

Posted on July 27, 2015 at 16:51Hi All,Why the ADC is work only with the following configuration :RCC_ADCCLKConfig(RCC_ADC12PLLCLK_Div4); ADC_CommonInitStructure.ADC_Clock = ADC_Clock_SynClkModeDiv4;I try to configure as the following:RCC_HCLKConfig...

ilanh by Associate II
  • 2673 Views
  • 8 replies
  • 0 kudos

STLink Error

Posted on July 30, 2015 at 02:43 I have previously been developing ok using ST-Util for mac and an STM32F103 board ( i have several of these basic boards) but recently the device stopped being detected and does not work on the offic...

0690X00000605IsQAI.png 0690X000006033MQAQ.jpg
mitch by Associate
  • 2328 Views
  • 2 replies
  • 0 kudos