cancel
Showing results for 
Search instead for 
Did you mean: 

Rise time of SPI Signal

hossam
Associate II
Posted on February 10, 2015 at 10:50

Hi

I am using STM32F103

RBT6

@72MHZ

I use SPI with DMA to stream data from memory to GPIO

SPI Prescaler is 4

GPIO is configured as output push-pull and speed 50MHz

The problem is that the data output rise and fall time is very slow, instead of getting square wave out of the scope for 0xAA data I get sine wave ''snapshot attached''

How I can get square wave with good rise and fall time at this frequency?

Salam

Hossam Alzmor

#gpio-risetime
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
AvaTar
Lead
Posted on February 10, 2015 at 12:26

This is not a problem of GPIO initialisation (this MHz value is only for glitch filtering), but of your PCB layout.

More exactly, the

https://en.wikipedia.org/wiki/Characteristic_impedance

of your slave connection.