STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F7x6 .net micro framework support

Posted on July 31, 2015 at 15:51Hello,Is there any plan to serve supporting documents and tools for .net micro framework support/port for the STM32746G-EVAL kit and/or STM32F7x6 MCUs? #.net-micro-framework-stm32f7

stm32f338 ADC problem

Posted on July 31, 2015 at 14:46 Hello I have problem with ADC of stm32f3 ; it seems if I read multiple times ; some reading return zero or the old reading ; I read the ADC every 200uSec ; for example delay(200usec) read_...

STM32F51K8 - UART Receiving using HAL libraries

Posted on July 29, 2015 at 17:29Hello,I'm working on a STM32F051K8 using the HAL libraries (with CubeMX).The MCU is connected with a processor through an UART link.I'm currently able to send characters strings withouth any problem using the normal m...

STM32F0 input capture ( CCR1 stays 0)

Posted on July 30, 2015 at 14:17Hello I generated code using CubeMX in order to measure a pulse (20µs - 100ms). TIM2 is what I am using for that. In the HAL_TIM_IC_CaptureCallback I am checking the value in the CCR1 register. I am expecting that in...

Timer counter clock divide

Posted on March 22, 2013 at 16:28 Hi, does some one know how to reduce timer counter clock? I need to measure some pulse width around 1ms using 16bit timer. I have already configured the timer but I get an overflow. TIM_...

vault by Associate
  • 4772 Views
  • 10 replies
  • 0 kudos

STM32F4 does not self-reset on power up; BOOT0 is tied to GND

Posted on April 16, 2013 at 22:58Hello, I'm using an STM32F415 in an LQFP64 package on a new PCB design. BOOT0 is tied to ground. I can program the STM32 (using IAR and the ISP designed by ST) and get it to run using the IDE. The NRST pin is floatin...

geof by Associate II
  • 8701 Views
  • 19 replies
  • 0 kudos

St-link Error in HEX parser

Posted on April 23, 2015 at 18:22Hi folks!I found a serious error in the ST-Link v3.6 parser.I have a project with the https://launchpad.net/gcc-arm-embedded 4.9-2014q4 toolchain.It generates a valid intel hex file, whit the small quirk, that there ...

0690X0000060316QAA.jpg
rigomate2 by Associate III
  • 3008 Views
  • 3 replies
  • 0 kudos

ST-Link Utility HEX bug ?

Posted on June 19, 2015 at 19:15Hi All Using ST-Link 3.6.0 to download a HEX file to an STM32F407 board I found that the loaded code sometimes didn't run. But, if I loaded the BIN version instead it was OK. After some investigation I found that the ...

hpipon957 by Associate III
  • 2536 Views
  • 7 replies
  • 0 kudos

ST Link Utility 3.7

Posted on July 11, 2015 at 08:18Hi to all,According to the release notes of ST Link Utility, the latest release is 3.7. This release supports STM32F7x development boards (like the discovery one). But, at the moment it's possibile to download only th...

carmine by Associate II
  • 2817 Views
  • 8 replies
  • 0 kudos