STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problem setting reload value for independent watchdog

Posted on July 29, 2015 at 16:47 Hi all, I am using a STM32F103 MCU and I want to set the reload value for independent watchdog (IWDG) so watchdog will reset the device (a timeout will occur) after ''t'' seconds. I am using the following code to ini...

danesh by Associate II
  • 3740 Views
  • 7 replies
  • 0 kudos

STM32F103 RTC Issues

Posted on July 27, 2015 at 10:20 Hello I am trying to configure the RTC of a cheap ARM board with STM32F103C8T6: http://www.ebay.co.uk/itm/High-Quality-STM32F103C8T6-ARM-STM32-Development-Board-Module-For-Arduino-Tool-/251621420724. I...

tbnkr by Associate II
  • 4846 Views
  • 8 replies
  • 0 kudos

Would like to enter DFU mode programmatically (on STM32F7)

Posted on July 28, 2015 at 03:27Hi, I have some code for entering DFU mode from my application which works on the STM32F4: https://github.com/micropython/micropython/blob/master/stmhal/modpyb.c#L70-L87 I'd like to do something equivalent on the STM3...

dhylands by Associate
  • 1494 Views
  • 2 replies
  • 0 kudos

Resetting over SWD without nRST in standby mode

Posted on July 29, 2015 at 16:59Hi, I have an STM32L15x. Is it possible to reset the microcontroller only over SWCLK and SWDIO without the reset pin when the microcontroller is in standby mode? I can access the target ID over SWD even though the dev...

Need EXplanation for a single line

Posted on July 29, 2015 at 15:07i have done bootloader and its jumps. but i like to know what the below line exactly does, Can anyone explain exactly why we give  0x2FFE0000 and do ''and '' mask and how it works?  if (((*(__IO uint32_t*)APPLICATION_...

arunl4g by Associate II
  • 824 Views
  • 1 replies
  • 0 kudos

FreeRTOS and HAL driver timeout issue

Posted on November 21, 2014 at 19:54Hello, in xPortStartScheduler routine, the systick priority is forced to /* Make PendSV and SysTick the lowest priority interrupts. */ Some HAL interrupt drivers implement a time out based upon systick value. Wi...

stst9193 by Associate II
  • 6488 Views
  • 9 replies
  • 0 kudos

NUCLEO-F302R8 RAM Shortage

Posted on July 29, 2015 at 16:14I've been developing on a NUCLEO-F302R8 but a recent change to the scope of the project has left me with a requirement for 40kB of RAM, and the part on this dev board only has 16kB. What's the best way to expand my RA...

daniel2 by Associate II
  • 1149 Views
  • 1 replies
  • 0 kudos

system clock stm32f0 ?

Posted on July 29, 2015 at 16:08hi' i'm new stm32f0 user and i working on stm32f072 , my first question what is value of system clock of microcontroller when i use system_stm32f0xx.c file which found in stm32f0_stdperiph_lib\STM32F0xx_StdPeriph_Lib_...

Migrating F411 project to L476 in Cube tool.

Posted on July 28, 2015 at 12:43Hi,  I have been developing my S/W using a F411 Disco board. For the end product, I need to use the L476 device. So is there a way of migrating between the 2 devices, either within or outside the Cube tool ?. I'd pre...

Pevy.Andy by Associate III
  • 1046 Views
  • 1 replies
  • 0 kudos