STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4 configuring exti port interrupt at one function

Posted on August 02, 2015 at 23:46 I configured `gpio` and `exti` handler configurations for 8 pins `(PD8,PD9...PD15)` each has separate configuration functions and it's working well. Can i do the configurations at just one function? Some lines ...

Stm32f1 cube and rtc problem

Posted on May 17, 2015 at 18:38When I set RTC date , rtc counter do not change. when turn on again my board   date to 2000/1/1 Stm32f103zc + cube

HAL Timer interrupt

Posted on July 30, 2015 at 19:24 Hello, I tried to use the Timer interrupt. In the examples of the STM Discovery they used the HAL_TIM_PeriodElapsedCallback handle function. But with this does'nt work (The don't used HAL_NVIC_EnableIRQ(T...

NUCLEO STM32F091RC - program doesn't run

Posted on August 02, 2015 at 09:56Hello. Program flashed with ST-LINK and Keil uVision 5.1 without any errors. The problem is program start only after several resets.  Anyone had similar problem? Thanks for any advice.

STM32CubeMX 4.9.0 and FW1.7.0

Posted on July 23, 2015 at 16:07Hey guys, does STM32F4, V1.7.0 work with CubeMX4.9.0? I have CubeMX4.7.0 and only can use FW V1.5.0 (known bug I know), so trying to determine if I should update to CubeMX4.9.0.....

bdesantis by Associate II
  • 1275 Views
  • 1 replies
  • 0 kudos

STM32F072 lowest PCLK is 10MHz?

Posted on July 31, 2015 at 12:26We have a design with STM32F072, and we would like to work with HSI at 8MHz in order to achieve the lowest posible consumption as long as we don't need too much processing power, thus the USB requiring 48MHz would be ...

Stm32f7xx internal flash size

Posted on July 31, 2015 at 09:03Hello.There is a question about stm32f7xx internal flash size. Will be released stm32f7 controllers with 2mb flash? There is only stm32f7 controllers with 1mb flash now. Anybody know?

STM32F401 SPI problem

Posted on July 30, 2015 at 06:45I work the SPI1 normally,but cannot work on other 2,3,4....i think F401 have SPI2,3,4 right?i via dma and setting follow my setting in SPI1i try SPI4, DMA channel 5 stream 3,4 for tx rx. but no output.the stdperiph li...

gillbike by Associate II
  • 3056 Views
  • 7 replies
  • 0 kudos

HardFault_Handler headache

Posted on July 30, 2015 at 10:36Hello all ; I have an old working project that we use  the function : arm_cfft_radix4_f32(&S, testInput); where testInput is a float array in the RAM . we need to add some function for the project we added more ext...