cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F4 USB VCP problem with timeout when send data from PC to device

jsi
Associate II
Posted on January 18, 2015 at 12:11

Hello.

I am use example VCP from the ST. on STM32f405

I am working under WinXP with a virtual COM port via the API as a file.

Cyclically sends data (short packets from 8 to 16 bytes) from PC to Device by function - WriteFile.

Data transfer immediately, but from time to time there is a strange TimeOut to transfer (WriteFile) sometimes up to 500ms.

Same work, but with a real COM port, such delays are not present.

What could be the problem?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0