STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F405 Odd DFU behaviour

Posted on August 18, 2015 at 16:47I'm experiencing some odd behaviour when attempting to place an STM32F405 into DFU mode. Currently, what works on one peice of hardware is that is that I send the STM32 a command to tell it to go into DFU mode, and ...

Audio stream STM32F4 disco

Posted on August 24, 2015 at 11:48The original post was too long to process during our migration. Please click on the attachment to read the original post.

matas by Associate II
  • 809 Views
  • 1 replies
  • 0 kudos

STM32CubeMX - Missing pins in MX_GPIO_Init

Posted on August 18, 2015 at 00:11 I'm having a problem getting all the pins to show up in the generated code from STM32CubeMX. Here's what I'm seeing: I'm generating a project using STM32CubeMx (v4.9.0) for the STM32F3348DISCOVERY board...

tristan2 by Associate
  • 1250 Views
  • 1 replies
  • 0 kudos

.

Posted on August 22, 2015 at 19:18. #sai-audio-codec #stm32f7

Frequency Measuring

Posted on August 20, 2015 at 15:26Hi ,Please i have to measure frequency from 1Hz to 3Khz with timer 1 (16bits)My SysTick clk = 72Mhz, so i set the prescalor to (1000-1) .So i have a Counter Clock=72Kand than i can capture frequency starting from 1H...

nechi by Associate III
  • 1951 Views
  • 8 replies
  • 0 kudos

fsmc timing

Posted on January 06, 2014 at 15:50 how he calculate this So, we will have the following FSMC timings: ? Address setup time: 0x1 ? Address hold time: 0x0 ? Data setup time: 0x5 #too-vague

0690X000006052pQAA.png 0690X000006052uQAA.png
elec_st by Associate III
  • 3684 Views
  • 9 replies
  • 0 kudos

STM32F407 + DSP from STM32Cube_FW_F4_V1.7.0

Posted on August 20, 2015 at 06:42Hello! I trying to create an aplication with FFT. So, I read 1024 points from internal ADC (12 bit), sampling frequency 1024 Hz. Then I process them with FFT functions from DSP lib STM32Cube_FW_F4_V1.7.0.http://code...

0690X000006058mQAA.png

USART on STM32F4 using Arduino board

Posted on August 21, 2015 at 00:28 NOTE: edited by moderator on Oct 6th, 2016 Hello everyone, I just received my stm32f4 discovery board yesterday and it works well :). I managed to run a LED blinking example. I now want to display ...

ed_62 by Associate II
  • 2641 Views
  • 2 replies
  • 0 kudos

Programming external application with stm32 Discovery

Posted on August 23, 2015 at 17:32Hello,I'm trying to program an external prototype board that I made using the same MCU as on the Discovery (stm32f407VG) and am getting the following error:Error: Flash driver function execute timeout     Erase:    ...

azayetey by Associate II
  • 1831 Views
  • 4 replies
  • 0 kudos

Locked Nucleo L053R8?

Posted on August 22, 2015 at 16:10I was developing a system on the Nucleo board.  I then moved it to a custom proto PCB which I was programming from the Nucleo on-board ST Link.  Everything was great up to that point. When I reverted back to use the...

joe2399 by Associate II
  • 1151 Views
  • 2 replies
  • 0 kudos