User Activity

Posted on March 24, 2015 at 14:39I need to transmit 5 bytes and after strobe ''update pin'' on ad9951 over and over again with speed about 300-400khz. Start every time transmission for each 5 bytes and strobe on tx complete - will not make it, it's ...
Posted on April 04, 2014 at 17:40After days spent in tries to connect adc via i2s - mcu stopped working. I can write and read flash via st-link, mcu is properly detected but it does nothing. Tried mass erase - did not helped.It seems that works only...
Posted on April 02, 2014 at 12:05hello everyonei have adc ad1877, configured as in pictureHow i should configure i2s in stm32f4 ? I have tried this one   I2S_InitStructure.I2S_AudioFreq = I2S_AudioFreq_32k;  I2S_InitStructure.I2S_Standard = I2S_Stan...