cancel
Showing results for 
Search instead for 
Did you mean: 

programming SPI on STM32F091RC

raphael
Associate II
Posted on April 22, 2015 at 17:02

Hi everyone,

I'm trying to program the SPI2 of my STM32 to only transmit data at 18Mbit/s as I saw on datasheet.

My problem is to configure the ''SPI_HandleTypeDef'' in order to use the function :

HAL_StatusTypeDef HAL_SPI_Transmit(SPI_HandleTypeDef *hspi, uint8_t *pData, uint16_t Size, uint32_t Timeout);

As I want to only transmit I don't know what to put into the following fields of the SPI_HandleTypeDef :

 uint8_t               *pTxBuffPtr;           /* Pointer to SPI Tx transfer Buffer */

  uint16_t               TxXferSize;           /* SPI Tx Transfer size */

  uint16_t               TxXferCount;          /* SPI Tx Transfer Counter */

  uint8_t               *pRxBuffPtr;           /* Pointer to SPI Rx transfer Buffer */

  uint16_t                RxXferSize;          /* SPI Rx Transfer size */

  uint16_t               RxXferCount;          /* SPI Rx Transfer Counter */

  uint32_t                   CRCSize;          /* SPI CRC size used for the transfer */

  void (*RxISR)(struct __SPI_HandleTypeDef *hspi); /* function pointer on Rx IRQ handler   */

  void (*TxISR)(struct __SPI_HandleTypeDef *hspi); /* function pointer on Tx IRQ handler   */

  DMA_HandleTypeDef          *hdmatx;          /* SPI Tx DMA Handle parameters   *

  DMA_HandleTypeDef          *hdmarx;          /* SPI Rx DMA Handle parameters   */

  HAL_LockTypeDef               Lock;          /* Locking object                 */

  HAL_SPI_StateTypeDef         State;          /* SPI communication state        */

  HAL_SPI_ErrorTypeDef     ErrorCode;         /* SPI Error code                 */

Here you have my main :

#include ''stm32f0xx.h''

#include ''system_stm32f0xx.h''

#include ''stm32f0xx_hal_rcc.h''

#include ''stm32f0xx_hal_spi.h''

int main(void)

{

    

    /***** Variables *****/

    uint32_t Freq_syst;

    HAL_StatusTypeDef SPI_status;

    SPI_HandleTypeDef SPI_handle;

    SPI_InitTypeDef SPI_init_struct;

    

    SPI_init_struct.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_2;

    SPI_init_struct.CLKPhase = SPI_POLARITY_LOW;

    SPI_init_struct.CRCCalculation = SPI_CRCCALCULATION_DISABLED;

    SPI_init_struct.DataSize = SPI_DATASIZE_16BIT;

    SPI_init_struct.Direction = SPI_DIRECTION_1LINE;

    SPI_init_struct.FirstBit = SPI_FIRSTBIT_LSB; //peut être mettre MSB first

    SPI_init_struct.Mode = SPI_MODE_MASTER;

    SPI_init_struct.NSS = SPI_NSS_SOFT;

    SPI_init_struct.NSSPMode = SPI_NSS_PULSE_DISABLED;

    SPI_init_struct.TIMode = SPI_TIMODE_ENABLED;

    

    SPI_handle.Instance = SPI2;

    SPI_handle.Init = SPI_init_struct;

    

    while(1)

    {

    }

}

Thank you for your help,
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0