STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Half cycle acces ob F1/F3

Posted on October 26, 2015 at 15:56Hello, what is Half-cycle access  (FLASH_ACR_HLFCYA) for? It may be used with slow clocks ( < 8 MHz)  and AHB divisior = 1.

I2C Problems

Posted on October 11, 2015 at 15:24 Hello, I tried to test the I2C interface on a STM32: #include <stdio.h> #include <stdlib.h> #include ''diag/Trace.h'' #include ''stm32f4xx_hal.h'' #include ''stdint.h'' int main( int argc,...

UART_DMA Delay ?

Posted on October 26, 2015 at 20:20Hi,I  have connected two MCU's through UART.I want to send a string from MCU 1 to MCU 2.once the MCU 1 sent the string it need to wait for some time to receive the reply from MCU 2.If MCU 1 did not get any reply fr...

Searching working example USB-Host with usb drive

Posted on October 08, 2015 at 10:48Hello, I failed to get an application with USB-Host and FatFS working with CubeMX. Does anyone has an example project? FatFS always reports fr_disk_error. I founds some posts with similar problems in some boards bu...

Merge SDIO with FATFS

Posted on October 21, 2015 at 13:33Hi,I have created a sdio and i would like to know how to merge the FATFS file system with the SDIO. I have seen some examples but  i am not understanding how the they give a link between file system module and SDIO...

arunease by Associate II
  • 3030 Views
  • 10 replies
  • 0 kudos

SDRAM STM32F429 FMC SDRAM DELAY

Posted on May 10, 2015 at 22:47The original post was too long to process during our migration. Please click on the attachment to read the original post.

Use USB CDC with DMA?

Posted on October 23, 2015 at 17:49Is there a way to use the USB stack of the F4Disco with DMA? I'd like to transfer some 100 bytes and then trigger an interrupt... At the moment I'm using UART with a USB-UART bridge for that.

Leonelf by Associate II
  • 3272 Views
  • 1 replies
  • 1 kudos