Posted on May 10, 2015 at 22:48The original post was too long to process during our migration. Please click on the attachment to read the original post.
Posted on May 10, 2015 at 22:47The original post was too long to process during our migration. Please click on the attachment to read the original post.
Posted on May 12, 2015 at 13:36after first change of value it looks like:Adress value------2002ffe4 ccccccccd0000000 ecccecccand after couple minutes2002ffe4 ccccccccd0000000 fcccfcccwhen i connected the D13 or D14 pins to the 0 or 1 i saw just ad...
Posted on May 11, 2015 at 20:59datasheet says ''Refresh Interval Time - max 15.6 '' so : //15.6us*84MHz=1311 when i use 100 FMC_Bank5_6->SDRTR=100<<1;this didnt gave any result.when i put even FMC_Bank5_6->SDRTR=10000<<1;thats didnt gave any re...
Posted on May 11, 2015 at 20:46datasheet says ''Refresh Interval Time - max 15.6 '' so : //15.6us*84MHz=1311 when i use 100 FMC_Bank5_6->SDRTR=100<<1;this didnt gave any result.when i put even FMC_Bank5_6->SDRTR=10000<<1;thats didnt gave any re...
Posted on May 10, 2015 at 22:53Hey did you solve this problem ? i have simmilar one with AS4C4M16S-6TIN. but after delay i have following results:2002ffd8 de111206d00003d4 fe117206so as you can see two octets are changed and i have no ideal what ...