STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32f207zg i2c, start bit error

Posted on October 21, 2015 at 15:54 Hi, I'm working on a custom board, cpu :stm32f207zg on i2c2 there is an rtc - pcf2129 I started the project in STM32CubeMX, updated to the last version. Pins are pf0 and pf1, pin...

sukoy27k by Associate II
  • 2039 Views
  • 3 replies
  • 0 kudos

DMA and EEPROM interference on STM32L1?

Posted on October 29, 2015 at 09:00I'm having a big problem.I have an USART which uses a circular buffer with DMA to receive characters.The machine sometimes has to save some informations in internal EEPROM.After some time, from minutes to many hour...

giuseppe by Associate II
  • 653 Views
  • 0 replies
  • 0 kudos

Pin value of a GPIO pin set as high impedance

Posted on October 28, 2015 at 08:49 I am using an STM32F4 discovery board and my intention is to set one of its GPIO pins at high impedance, which I have done as below: GPIO_InitStruct.Pin = GPIO_PIN_12; GPIO_InitStruct.Mode = GPIO_MODE_INPUT;...

sommer by Associate II
  • 10254 Views
  • 3 replies
  • 0 kudos

Reading wrong Temperature sensor values stm32f0

Posted on October 29, 2015 at 08:47Hi,I am using STM32F051R8 eval board I am trying to read temperature sensor and internal voltage values but some times I am getting wrong ADC conversion valuesvoid MX_ADC_Init(void){  ADC_ChannelConfTypeDef sConfig...

TJpgDec and FatFs

Posted on October 26, 2015 at 09:51 I checked the code, it works when picture is in memory. But I can't make it work with MicroCD. I rewrote the code for work with FatFs, but STM32 freezes on f_lseek() function. There is my code, I purpo...

STemWin and RTOS

Posted on October 25, 2015 at 18:59is there is any example of STemWin using FreeRTOS? I am using discovery kit STM32F429 I have my main function has only GUI_Init(); I keep getting this error  region `RAM' overflowed by 1919320 bytes

smhhadima by Associate II
  • 1209 Views
  • 3 replies
  • 0 kudos

Problem with copying hex data

Posted on October 28, 2015 at 13:28 Hello, I have following problem with copying hex data. for (i = 0; i < 6; i++) { printf ( ''%02x'' , packet[i]); // copy packet to FIFO } Printf copy data from packet[] to FIFO...

hospodar by Associate III
  • 1504 Views
  • 2 replies
  • 0 kudos

Storage Format For Multiple Sensors: STM32 Datalogger

Posted on October 28, 2015 at 14:20Hi,I am working with a STM32 data logger with a pulse counter, SPI accelerometer and ADC connected. I am puzzled: how can I design a common 4/8Kb buffer for time-synchronous sensor values for later SDIO SDcard stor...

avashalo by Associate II
  • 2234 Views
  • 5 replies
  • 0 kudos

Using 2 comparator for the same signal

Posted on October 28, 2015 at 19:36Hi everyone,MCU: STM32F302I have to configure 2 differents analog comparators (Comparator 1 and comparator 2). Each comparator are linked internally to TIM1_OCRefClear. Is that a problem to control the same signal ...

jf2 by Associate II
  • 761 Views
  • 0 replies
  • 0 kudos