STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32VL discovery FAT drive

Posted on October 29, 2015 at 14:02When I plugged the STM32VL discovery board in a PC, there will be a ''removable drive'' in the Computer, and there are some internet shortcut in it. The Win says that it is formatted to FAT, and the free space is a...

lac by Associate II
  • 2441 Views
  • 5 replies
  • 0 kudos

Std Periph Lib --> Project Setup / Debug

Posted on October 29, 2015 at 17:46HelloCurrently i work with the HAL lib where i can graphically setup the system clock of my STM32F4xx controller. I do have to set up the same libraries i wrote (mostly copy paste except interface commands,.. ) in ...

stm3f334 with software spi

Posted on October 29, 2015 at 17:05 hello all ; I need to use a software SPI in stm32f334 @ 72Mhz ; the maximum software SPI I can get is 1Mhz ; but I need 4 MHZ SPI ; could you tell me how to do that please ? here my code that I...

Enter stop-mode from PVD interrupt

Posted on October 29, 2015 at 17:13If i place my enter ''stop code'' into PVD interrupt I can enter stop mode but not exit. If i place the same code outside the PVD interrupt (in the while(1)) I can both enter and exit stop mode. I use STM32L053. if...

purkovic by Associate II
  • 771 Views
  • 0 replies
  • 0 kudos

UART frame error, STM32L476, HAL

Posted on October 29, 2015 at 16:58Hello. I have configured a UART using HAL. For most things, the same Setup that I've already had working when using blocking mode, using Transmit only. But now I tried to use Receive also. When the program starts t...

Stm32F0 I2C comunication trouble

Posted on October 29, 2015 at 15:02What is wrong here?I try to read 2 bytes data of temperature sensor LM73 by I2C of STM32F0Discovery based on STM32F051 micro. The micro is waiting RXNE event and doesn't exit from the loop.I don't see any activity ...

STM32F100RC Missing TIM12-17

Posted on March 28, 2015 at 17:59Hello.I try enable TIM12-17 but TIM12EN-TIM17EN not set to 1 (always 0) in APB1ENR and APB2ENR.?an you help me?Thanks. #stm32f100rc

ankuch by Associate II
  • 5400 Views
  • 13 replies
  • 0 kudos

About the SAI duplex mode of STM32F746

Posted on October 29, 2015 at 10:56Hi,my friend, I want to implement the both TX/RX channel of SAI, but can not find any code sample in STM32CUBE. I want to use DMA to transfer audio data between SAI and codec and start the TX/RX DMA at once and jus...