STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX USB HS Mass Storage Class code 10

Posted on June 17, 2015 at 09:34 Hi, I have an STM3240G-EVAL board and I try to configure the USB-HS with the SD-Card. I have seleccted: - USB-OTG-HS: External Phy - Device_Only - SDIO: Mode - SD 1 bit - USB_DEVICE: C...

stock23 by Associate II
  • 1846 Views
  • 3 replies
  • 0 kudos

Weird Measured Power Curve for the Stm32f407 Discovery Kit

Posted on December 04, 2015 at 19:22Hi, In a goal of a personal project, i am trying to profile energy consumption of an ARM MCU board, so i take the ''stm32F407 discovery kit'' as an experiment example.In my power measurement experiment i always ge...

nadir by Associate
  • 693 Views
  • 1 replies
  • 0 kudos

Problems with input capture on Nucleo152RE

Posted on December 04, 2015 at 16:46I am working on a Nucleo152RE using EmBitz. The code generates a PWM signal (200Hz 50% duty-cycle) on PB8 (TIM4 channel 3) (It works, I tested with an oscilloscope), then gives this signal as input to PC6 (TIM3 ch...

stm32f427 flash dual bank IAP, random hard faults

Posted on December 04, 2015 at 15:06Hello,I am working on in-application programming of STM32F427, 1MB flash. I have set the DB1M bit in the flash option control register, so the flash memory is organized as two banks of 512 Kbytes each. I am trying...

RTC on STM32F746G-DISCO Ploblem

Posted on December 05, 2015 at 09:10Hi I'm trying to get the RTC work on STM32F746G-DISCO Board. The problem I'm facing is the calendar counter except SubSeconds stop counting after calling the function HAL_RTC_GetTime() since the first time. I've t...

gtopba by Associate II
  • 647 Views
  • 0 replies
  • 0 kudos

CubeMX 4.11.0 USB Custom HID problem.

Posted on December 04, 2015 at 09:47Today I've updated CubeMX to 4.11.0 version and library for L0 series to 1.3.0 version. I wrote a Project include USB Custom HID, ADC , DAC ... everything work fine except USB Custom HID. It work but speed is too ...

stm32f4 screen rotation

Posted on December 03, 2015 at 10:19Hello. I use ltdc interface to communicate with 800*480 tft screen. I need to rotate the image by -90 degress. Is it possible to do it by hardware? Software do it too slow.

STM32Cube and FreeRTOS - only 1st spawned task runs

Posted on December 04, 2015 at 00:15Hi, I'm new to using both STM32Cube and the FreeRTOS it provides support for, and I am trying to follow the tutorials and the FreeRTOS manuals online to create  2 separate tasks to manage the two I2C busses on our...

dean by Associate II
  • 3230 Views
  • 4 replies
  • 0 kudos

question about the SAI clock and example in cubeL4

Posted on December 04, 2015 at 07:07for the SAI example in cubeL4, it looks like running 22050 sample rate, and the input clock is 11.294M. I measure the frame len is about 45us which is 1/22050. Now I develop an audio app runs 44100,  I have checke...

jiangpen by Associate II
  • 1092 Views
  • 2 replies
  • 0 kudos