STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F7 24-Bit TFT and SDRAM (No DQM lines)

Posted on December 13, 2015 at 21:16Hi guys, I am using the STM32F746ZGT6 with a 24Bit RGB-TFT and an external SDRAM memory. In CubeMX I have seen, that I cant use the DQM lines together with the full 24-Bit wide bus for the TFT. I want to use the ...

dennis23 by Associate II
  • 1455 Views
  • 2 replies
  • 0 kudos

DFU through USB Memory Issue

Posted on December 16, 2015 at 10:20I've been trying to upgrade the firmware on my STM32F105 project by using DFU through USB. The problem is that I need to read ADC using DMA for both the boot code (to check whether some switches are set right to a...

could not able to compile code in keil

Posted on December 16, 2015 at 19:50Hi,i m using stm32f103 nucleo board and keil compiler. I downloaded code from keil website for uart. and tried to compile the code but got error as some files are missing. following are the errors.C:\Keil_v5\ARM\P...

SS.Sagar by Associate III
  • 2637 Views
  • 4 replies
  • 0 kudos

STM32CubeMX Bug in Code Generation for NucleoF072

Posted on December 15, 2015 at 19:10There is a defect in the initialisation code that STM32CubeMZ generates for an STM32F072RB target if the high-speed external clock is selected.  For some reason the code expects a value for constant 'HSI48_VALUE...

How to write to internal Flash memory?

Posted on December 17, 2015 at 14:32I am working with an ST http://www.st.com/web/catalog/tools/FM116/SC959/SS1532/PF258515?sc=stm32l152c-discovery board (STM32L152RCT6). I have been able to program the device and do all entry level things. Now I wa...

0690X00000605BEQAY.png

STM32F429I DISCO LCD Help

Posted on December 17, 2015 at 14:03 Hi Guys. I recently picked up the above-mentioned evaluation board. I am currently using TrueStudio. I want to display text strings on the on-board LCD. I have been trying to butcher o...

abotha by Associate III
  • 1086 Views
  • 1 replies
  • 0 kudos

usbd_storage.c (MSC class) supports multiple LUN?

Posted on December 16, 2015 at 03:10Hi All,Does anyone know if the STM32 USB device library MSC class support more than 1 LUN? I can get 1 LUN to work fine using either external flash or a uSD card. But when I tried to set STORAGE_LUN_NBR to 2 and h...

xxc2rxx by Associate II
  • 3023 Views
  • 4 replies
  • 1 kudos