Question
Using SD Card with STM32L152C Discovery
Posted on July 08, 2015 at 09:25
I have a STM32L152C Discovery board. I want to use a 1GB FAT SD Card with STM32Cube and EWARM ide, but there is an error.
pins: STM --- SD Module PA5 SCK PA4 CS MISO MISO MOSI MOSI Ext_3V 3.3V GND GND I started STM32Cube, Selected my board ''STM32L152C-DISCO'' in board selector. I checked FATFS->User-defined check box. RCC.High Speed Clock (HSE) -> Crystal/Ceramic Resonator SPI1->Full-Duplex Master And I Created EWARM project. f_mount() returns 0 and f_open() returns 13, even if I disconnect my sd card from sd module! int main(void) { printf(''Starting ...\n''); GPIO_PinState pinState = HAL_GPIO_ReadPin(GPIOA, GPIO_PIN_15); HAL_GPIO_WritePin(GPIOA, GPIO_PIN_15, GPIO_PIN_RESET); /* Reset of all peripherals, Initializes the Flash interface and the Systick. */ HAL_Init(); /* Configure the system clock */ SystemClock_Config(); /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_SPI1_Init(); MX_FATFS_Init(); FATFS SDFatFs; // File system object for SD card logical drive FIL MyFile; // File object volatile FRESULT res; // FatFs function common result code res = f_mount(&SDFatFs, ''0:'', 0); // returns 0 if(res != FR_OK) printf(''f_mount Error : %d\n'', res); // there is no error else { printf(''f_mount OK\n''); res = f_open(&MyFile, ''file.txt'', FA_CREATE_ALWAYS | FA_WRITE); // returns 13 if(res != FR_OK) printf(''f_open Error : %d\n'', res); // f_open Error : 13 else { printf(''f_open OK\n''); f_close(&MyFile); printf(''file opened.''); } f_mount(0, '''', 1); } } #stm32l152c-sd-fatfs