STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32L051 Comparator input impedance

Posted on March 23, 2016 at 15:11Hello, I'd like to monitor battery voltage (V~8volts) using comparator and voltage devider with two resistors (1-10M). Coud you please specify analog comparator input impedance, so i can select appropriate resistor v...

mailbox by Associate II
  • 1633 Views
  • 2 replies
  • 0 kudos

STM32F4DISCOVERY - IoT Multiple LCDs

Posted on March 24, 2016 at 04:48Hi I had a couple of questions. I'm from the software side of things and hardware is new to me!I am starting a project where I'd like to drive around 5 colour lcd's.It's a bit tricky in that I'd ideally like a mobile...

penny by Associate
  • 740 Views
  • 0 replies
  • 0 kudos

STPM10: Reactive and Total Harmonic Distortion

Posted on March 23, 2016 at 20:34Hi, first of all I'm sorry for the offtopic, but there is no smart meter IC section on the entire forum, which is odd.I've a functional prototype of a Smart Meter running on a STM32-F0/STPM10 platform. Before enterin...

royconejo by Associate II
  • 2065 Views
  • 4 replies
  • 0 kudos

Bug in STM32Cube for STM32F417

Posted on February 27, 2014 at 21:56Hi, If you set the PLL speed of the micro to 160MHz (PLL_M=25, PLL_N=320, PLL_P=2) then the generated software correctly contains the line in SystemClock_Config():   HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_L...

rgledhill by Associate II
  • 3273 Views
  • 9 replies
  • 0 kudos

Unable to program when in stop mode

Posted on March 22, 2016 at 18:41I'm unable to program a STM32 using the STLink2 when the micro has firmware running that puts it into stop mode.I've played with the reset sequence settings in Keil but none of them solve my problem.Does anyone know ...

bluscape by Associate III
  • 2171 Views
  • 3 replies
  • 0 kudos

STM32F4 Dual ADC Reg Sim Mode with DMA

Posted on March 21, 2016 at 18:02 Hello, I want to read ADC1 CH0 and ADC2 CH1 in dual regular simultaneous mode and buffer it in DMA. I want to send the ADC values via UART to my PC and read them from the COM Port. When I start the program n...

LTDC is DMA?

Posted on March 23, 2016 at 08:27Hi ,Can any one tell me,Whether LTDC is DMA or not?LTDC is basically working as blocking or non blocking?By Tamilselvan

Confused by STM32L4 datasheet max SPI clock frequencies

Posted on March 22, 2016 at 20:10I'd like to use an STM32L4 in a project where I am interfacing with a 1-MSPS, 16-bit SPI ADC (LTC2378-16).  Obviously the SPI clock has to be > 16 MHz to run this at full speed.  However, for best performance the clo...

mhaun by Associate II
  • 2933 Views
  • 2 replies
  • 0 kudos

sdio dma--emmc

Posted on March 21, 2016 at 10:13Hi i am using f4 and it works with the polling method. But it doesnot work on DMA.. i am getting SDIO_IT_RXOVERR error. Can anyone  help me ?

arunease by Associate II
  • 937 Views
  • 1 replies
  • 0 kudos