STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Troubles using Mx plugin

Posted on May 20, 2016 at 10:19Hi folks, I have installed MX plugin 4.14.0.201603171736 into an existing eclipse Mars.2 (4.5.2). Looks like it worked. But when I try to show an STM32CubeMX window, it simply crashes my eclipse. I was expecting being ...

STM32F103 I2C Slave strange behaviour [Solved]

Posted on May 16, 2016 at 15:24Hi,I have a STM32F103 MCU with I2C2 enabled and configured as slave (ID 0x28h). I also have a STM32F429 MCU with I2C3 as Master.I've found an Optimized I2C Examples on ST's website and I've used that as a base. All I a...

dman by Associate II
  • 1890 Views
  • 2 replies
  • 0 kudos

STM32F469I-Disco CAN Interfaces connections

Posted on May 19, 2016 at 09:42Hi, I have successfully connected and run the CAN2 interface on this board. Now, I'm trying to connect the CAN1 but I can not find the corresponding port pins on the board. I've been reading the pds but there is no inf...

STM32F407 High Speed GPIO (Internal Clock) can't get 42Mhz

Posted on May 18, 2016 at 17:52Hi,I can't get the GPIO into high speed as stated in data sheet 42Mhz with the following code even I already set the clock to Max based on Internal clock:RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE);GPIO_InitDe...

zhanwey by Associate II
  • 2347 Views
  • 5 replies
  • 0 kudos

Relation between JTAG/SWD and HCLK

Posted on May 19, 2016 at 11:50Hello, I am searching for hard facts about the clock relation requirements between the Core HCLK Clock and the external applied JTAG/SWD clock. Any hints welcome!

Bootloader sometimes run slow.

Posted on May 19, 2016 at 05:12Hi:   My systems run STM32F427@168 MHz using external oscillator @ 8 MHz. The system will first run boot-loader then jump to main application. I find that sometimes the boot-time is long. After check it's due to boot-l...

how to use BSP in general / IHM01A1

Posted on May 18, 2016 at 16:05Hello everybody, I am experimenting with an Nucleo-STMF030R8 and the X-Nucleo-IHM01A1 Expansion board. The example Project from STM32CubeExpansion-SPN1_V1.6.0 is working fine and i also managed to modify this Project. ...

STM32CubeMX Two VCPs using CDC

Posted on May 17, 2016 at 14:29I'm a beginner in USB Stack on STM32F4. I have a question about creating a project using CubeMX (STM32F4 Discovery) for USB CDC to have 2 Virtual Com Ports in the ''Device Manager'' ? Thanks