STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

WAV file to c array (audio_sample.c)

Posted on June 14, 2016 at 23:11Hi!, i'm trying to recreate the C array of the file ''artofgardens-instr '' that came as example in ''audio_playback_and_record'' files, but with no luck.Does anyone knows how to do that kind of convertion?   from wav...

dracog71 by Associate II
  • 13926 Views
  • 9 replies
  • 0 kudos

No Carrige return when redirect printf() to UART2

Posted on June 15, 2016 at 15:41 Hi there, I'm working on custom board based on STM32F103 and the IDE is Keil. I will use UART2 to print some debug logs. To do this I add the fputc function to my code in order to redirect printf to...

Fede Rico by Associate III
  • 1559 Views
  • 3 replies
  • 0 kudos

sinus pwm wrong frequency

Posted on June 16, 2016 at 14:26Hi.I am using discovery board with STM32F100; I have made a code to generate a sinusoidal waveform through pwm via lookup table method.I think I miss something in computing the output frequency of the sine wave.Here i...

ionutF by Associate III
  • 1109 Views
  • 2 replies
  • 0 kudos

ADC continuous conversion STM32F103

Posted on June 16, 2016 at 16:43 I'm facing with a problem regarding continuous acquisition of ADC channel in STM32F I use the interrupt at the end of conversion to call a callback function to store the acquired value. The problem regards t...

Fede Rico by Associate III
  • 784 Views
  • 0 replies
  • 0 kudos

Interrupt Management

Posted on June 16, 2016 at 13:17Hello EveryoneI am trying to run my code on stm32f4, with use of interrupt routines. I have an 9dof imu including mpu6050,hmc588,bmp058. So i am interfacing 3 EXTI rsubroutine to read imu and this has been successfull...

Install u-boot on stm32f4 discovery board

Posted on June 15, 2016 at 17:43Hello guys, I'm trying to install u-boot on my development board STM32F407 . After loading the binary image, the UART1 interface does not work . I'm using the version available from the website emcraft for the board S...

rs23 by Associate II
  • 1242 Views
  • 1 replies
  • 0 kudos

HAL bug - array overflow in HAL_RCC_GetSysClockFreq()

Posted on June 10, 2016 at 17:23The purpose of this post is to save other developers the time I have spent tracking this down. Bear with me on this - its messy. Line 1108, of stm32f1xx_hal_rcc.c is  if (pllmul == aPLLMULFactorTable[(uint32_t)(RCC_...

UART DMA INT is not working

Posted on June 16, 2016 at 10:30 Hi, I'm facing a strange problem with UART DMA int in a FreeRTOS-based project. When I call the DMA setup function (below) from a given FreeRTOS task, it works just fine and the ISR is executed. However...

0690X00000605PtQAI.png
asaad by Associate
  • 759 Views
  • 0 replies
  • 0 kudos