STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F407xx SPI Slave usage - Polling method.

Posted on July 09, 2016 at 08:03I am working on establishing SPI communication between STM32F407ZET6 and NRF52832 chipsets.Currently, I am configuring STM32F407ZET6 is the slave as I need to send the data continuously from NRF52832.I found code in g...

Magnetometer

Posted on August 08, 2016 at 15:52Hello folks, I am trying to implement magnetomter LIS3MDL with STM32F4. After reading the X, Y and Z axis register I am getting negative values as they are 2's complement. How can I transmit them on UART to see nega...

stm32f10x - Input capture

Posted on August 05, 2016 at 21:15 Hi everyone, I'm using the stm32f10x to measure a pulse width and I followed the Input Capture example but I still have some errors. The measurement is erratic, sometimes the value is ok and most of the time...

fntheirs by Associate
  • 1984 Views
  • 3 replies
  • 0 kudos

USART polling vs Interrupt

Posted on August 08, 2016 at 14:12Hi,I have implemented simple USART polling and interrupt method.// main functionwhile(1) {  send_data(); //usartSendString(USART1,array,34); GPIOF->ODR ^= GPIO_Pin_10;   }///simple USART polling functionvoid usartS...

Niks by Associate II
  • 2088 Views
  • 4 replies
  • 0 kudos

[BUG] 32F746GDISCOVERY BSP LCDv

Posted on August 06, 2016 at 19:51 I'm not sure that this is the right place to signal a bug. However, I am working with the LCD embedded in the 32F746Discovery board. I noticed a strange behavior during experimentation with scrolling effects an...

STM32F103 Sweep frequency

Posted on August 05, 2016 at 07:50 Hi im newbie with this mcu, and im try to doing a sweep of frequency with TIM3 and the chanel1, A6. my main code its the next while (1) { unsigned int i=0, j=0, h=0; for(i = FrequencyStart; i < (Frequenc...

0690X00000602rDQAQ.jpg 0690X00000603AhQAI.jpg
woutnme by Associate II
  • 1220 Views
  • 1 replies
  • 0 kudos

Byuing evaluation tools from ST.

Posted on August 07, 2016 at 14:35I can not find any information about valid payment types and if  shipping is included.I like to use paypal for Internet payment.Can anyone enlighten me ?

itchef by Associate
  • 1128 Views
  • 1 replies
  • 0 kudos

STM32F407VGT6 programming and debugging

Posted on June 30, 2016 at 22:25Hello, I have developed my code using IAR workbench, tried it on STM32F4 discovery board and it worked well. Now I want to download the code on STM32F407VGT6 chip I bought from digikey.com directly without the develop...

I2C Problem - STM32F4 DISCOVERY

Posted on August 03, 2016 at 08:33Hello everyone. I have searched the forums but could not figure this out.I am using the STM32 F4 Discovery, AC6 (System Workbench), and the standard peripheral libraries.On the Discovery Kit PA8 (pin 100) should be ...