User Activity

Hi,I use custom USB device class implementation on top of ST's USB device stack (generated by CubeMX). I need only core implementation but i can not generate it without specifying some USB class from list in CubeMX!This is pretty annoying because i h...
Posted on May 24, 2016 at 15:41 Bug in file ''stm32f4xx_hal_dcmi.h'' at line 335: #define __HAL_DCMI_GET_FLAG(__HANDLE__, __FLAG__)\ ((((__FLAG__) & (DCMI_SR_INDEX|DCMI_MIS_INDEX)) == 0x0U)? ((__HANDLE__)->Instance->RIS & (__FLAG__)) ...
Posted on March 02, 2016 at 14:13 Hello, and the next SPI bug is insideHAL_SPI_TransmitReceive function. It hangs communication after a few bytes shifted over SPI. The reason is that code logic is broken (it was correct in previous librar...
Posted on February 29, 2016 at 14:46 Hello! After upgrading to latest version of cubemx (to 4.0) and updating HAL library to v1.0 my SPI code is broken in strage way - NSS pin state is igneored! My test setup: STM32F429VGT6 168 ...
Posted on February 20, 2016 at 14:51Hello and sorry for  my bad English )I have a problem with FS USB Device (Embedded PHY) on STM32F429VGT6 MCU. I implemented custom USB ''vendor device class'' on top of ST USBD Core library and custom communicatio...
Kudos given to