STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4 discovery + SSD1963

Posted on August 22, 2016 at 21:54The original post was too long to process during our migration. Please click on the attachment to read the original post.

bfeixas by Associate II
  • 1153 Views
  • 0 replies
  • 0 kudos

Documentation bug in RM0090 DocID018909 Rev 12?

Posted on August 22, 2016 at 20:20The reference manual for the STM32F4[05,15,07,17,27,37,29,39] in the section describing TIM1,8 has a block diagram (figure 86) that doesn't make sense.The CC1I interrupt is shown to be generated by channel 4, CC2I b...

Inserting delay before synchronized pwm signal

Posted on August 18, 2016 at 12:01Hi All,I have two signal, one high signal having 20% duty cycle and a low signal with 40% duty cycle. High signal is  synchronized to low signal with reset trigger. I want to insert a delay of 100-400ns (t2 in diagr...

0690X00000605OSQAY.png
nitin29 by Associate II
  • 1219 Views
  • 1 replies
  • 0 kudos

What wireless communication module with libraries (Wifi?)

Posted on August 21, 2016 at 19:38Is there a wireless module or chip with libraries. The possibility of an external antenna is a plus, in case of metal box. I tried NRF24 modules. they have libraries around the net but I could not get them to compil...

LMI2 by Lead
  • 1056 Views
  • 2 replies
  • 0 kudos

software expansion package for STM32Cube

Posted on October 07, 2015 at 14:20Hello,Does anyone know how to install a software expansion  package for STM32Cube. Let's say I downloaded X-CUBE-MEMS1.ZIP. I then went to ''Help/Install New Libraries'' then clicked on ''From Local...'' I selected...

STM32F0 SPI Timeout Error with illegal HAL state

Posted on August 19, 2016 at 12:28 Hello, [I have just written my issue in detail and it has been deleted when I clicked Ok. Thanks, I will write it again though.] We are using the STM32F072CB with the HAL driver in our application a...

janos2 by Associate II
  • 1740 Views
  • 4 replies
  • 0 kudos

Interrupts Don't Fire Up in HAL SPI

Posted on July 31, 2016 at 21:34The original post was too long to process during our migration. Please click on the attachment to read the original post.

nitin29 by Associate II
  • 1268 Views
  • 1 replies
  • 0 kudos

HAL_UART_Receive_IT returns error

Posted on August 04, 2016 at 09:48 Hi, I want to transmit something from PC to uC and I put UART in receive mode. However HAL_UART_Receive_IT keeps returning error, and I don't know why? My code is really simple: int main(void){/* Reset...