User Activity

Posted on March 10, 2015 at 11:21Hi All,I'm on the tail end of a large development for an stm32 using gcc and openocd. As I add more code and bitmaps (for the LCD) I'm finding the load times getting rather long, mainly due to the bitmaps.I'd therefo...
Posted on December 18, 2014 at 17:21Hi,Does anyone know if STM are going to continue developing the standard peripheral drivers for the foreseeable future? Or are they being superseded by by the Cube drivers?If if both will be running in parallel do...
Posted on January 31, 2014 at 17:31Hi,I am implementing a CDC USB device using the STM32f4 and STM USB libraries.What I am finding is that after sending a number of multi-byte packets from the PC > STM32 the OUT pipe effectively hangs and I receive ...
Posted on January 22, 2014 at 16:12Hi,From reading the documentation, I gathered that it is possible to use the high speed core with the embedded full speed phy. I understand that I'd be limited to full speed with this setup but I believe that with ...
Posted on January 22, 2014 at 12:34Hi,I have seen mentioned in the forum that ST have provided use of their Vendor ID, with a unique Product ID to people using their processors.I would like to ask how I could obtain a unique product ID for our compa...