erik2399
Associate
since
2018-07-19
2023-06-14
User statistics
1
Posts
0
Solutions
0
Kudos given
0
Kudos received
STMicroelectronics Community
About erik2399
Options
Report User
User Activity
Posts
Replies
STM32Cube Bug - HAL_RTCEx_SetWakeUpTimer_IT
2016-02-12
Posted on February 12, 2016 at 22:42 I'm using the HAL libraries to set up and control the RTC features of an STM32F3 device. The RTC is based on LSE, and is running fine. However, when enabling the wakeup timer, no interrupt was ever generated ...
No replies to display.