STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

HAl Library, difference between SW4 and CUBE ?

Posted on September 16, 2016 at 23:34Hello. This is my 1st post here. I'm trying to use a NUCLEO F103RB to make my own electronic application. I'm an electronician, not really a programmer. I've installed Eclipse OpenSTM (Mac OS X version), and I ca...

jihzed by Associate II
  • 953 Views
  • 0 replies
  • 0 kudos

ADC in dual simultanious mode

Posted on September 15, 2016 at 23:51Hello everyone! I have issue with initializing ADC1 and ADC2 in  regular simultanious mode + DMA. I am using CubeMx and Hal drivers. Here is my configuration.http://s8.picofile.com/file/8267541418/1.JPGhttp://s8....

pooyan by Associate
  • 1204 Views
  • 2 replies
  • 0 kudos

external interrupt is not generating on PB0 pin

Posted on September 16, 2016 at 20:17hi,i m trying to set the external interrupt for PB0 pin on rising or falling edge. i configured but it is not working properly.here is configuration i gave[CODE]&sharpdefine NVIC_PRIORITY_MASK(prio) ((prio) << (8...

SS.Sagar by Associate III
  • 916 Views
  • 1 replies
  • 0 kudos

SRAM parity error detection

Posted on September 15, 2016 at 23:55Hi.I would like to enable parity error detection for SRAM in STM32F303. I know that this is done through programming option bytes.But I don't know, how can I actually detect if parity error has occurred. If it ha...

matic by Associate III
  • 1469 Views
  • 2 replies
  • 0 kudos

STM32F0 ESD/EMI sensitivity

Posted on September 08, 2016 at 18:07Hello all.I've designed a board using microcontroller STM32F030K6 and face the problem with ESD immunity of this controller (as I suppouse).Our device consists of 4 boards (one based on STM32 and 3 others - on ST...

ap1011 by Associate
  • 1099 Views
  • 1 replies
  • 0 kudos

Mixed DMA RX, polled TX SPI

Posted on September 13, 2016 at 03:23I already know the HAL firmware doesn't support this but is this due to the bad programming of the HAL or inadequacies of the hardware?I'm interfacing to an external NOR flash device but have run out of DMA chann...

STM32 as SSI slave / Clearing SPI TX Fifo on F0

Posted on September 12, 2016 at 07:09Hi Everyone, I am currently trying to implement a SSI slave using a STM32F0(72RB) microcontroller. For those who are not familar with SSI: SSI is used as a sensor (encoder) interface for high speed applications (...

cschumann by Associate II
  • 1574 Views
  • 1 replies
  • 0 kudos

simpel tone / beep on stm32F7 with wm8994

Posted on August 05, 2015 at 22:25Hi guysI try to make a simpel sinusial tone / beep on the STM32F7-Discovery borad but can not find a solution.Do anybody have the time to show howto ?Hjalmar

hjh by Associate III
  • 1560 Views
  • 4 replies
  • 0 kudos

***non volatile memory --- STM32F107

Posted on August 31, 2016 at 17:36Previously, I worked on MSP430F47197. I learnt how to read/write from flash. That was pretty easy. On the other hand, using EEPROM was really confusing to read from and write into. (Using I2C Protocol)Now, I am work...